Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DrawBeadBuilder.OrientationTypes |
DrawBeadBuilder.OrientationTypes.ORTHOGONAL
The width and angle parameters are orthogonal, or normal, to the sheet metal normal at the section location.
|
static DrawBeadBuilder.OrientationTypes |
DrawBeadBuilder.OrientationTypes.VERTICAL
The width and angle parameters are oriented along the draw direction at the section location.
|
Modifier and Type | Method and Description |
---|---|
DrawBeadBuilder.OrientationTypes |
DrawBeadBuilder.baseOrientation()
Returns the orientation used to construct the sections representing the bead shape.
|
static DrawBeadBuilder.OrientationTypes |
DrawBeadBuilder.OrientationTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.OrientationTypes |
DrawBeadBuilder.OrientationTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.OrientationTypes[] |
DrawBeadBuilder.OrientationTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawBeadBuilder.setBaseOrientation(DrawBeadBuilder.OrientationTypes baseOrientation)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.