Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static ClearanceBuilder.ClearanceGeometryTypes |
ClearanceBuilder.ClearanceGeometryTypes.SECTION
The input is closed profiles.
|
static ClearanceBuilder.ClearanceGeometryTypes |
ClearanceBuilder.ClearanceGeometryTypes.SOLID
The input is solids.
|
Modifier and Type | Method and Description |
---|---|
ClearanceBuilder.ClearanceGeometryTypes |
ClearanceBuilder.clearanceGeometryType()
Returns the input type of the clearance geometry.
|
static ClearanceBuilder.ClearanceGeometryTypes |
ClearanceBuilder.ClearanceGeometryTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ClearanceBuilder.ClearanceGeometryTypes |
ClearanceBuilder.ClearanceGeometryTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ClearanceBuilder.ClearanceGeometryTypes[] |
ClearanceBuilder.ClearanceGeometryTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ClearanceBuilder.setClearanceGeometryType(ClearanceBuilder.ClearanceGeometryTypes clearanceGeometryType)
License requirements: ug_die_design ("Die Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.