Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Method and Description |
---|---|
DieAssistantTrimProfile |
DieAssistantTrimProfileList.findItem(int index)
Returns the object at the input index.
|
DieAssistantTrimProfile[] |
DieAssistantTrimProfileList.getContents()
Gets the contents of the entire list
License requirements: None. |
DieAssistantTrimProfile |
TrimFlangeDieAssistantBuilder.newTrimProfile()
Creates a new trim profile item in the set
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DieAssistantTrimProfileList.append(DieAssistantTrimProfile object)
Appends an object to the list
License requirements: None. |
void |
DieAssistantTrimProfileList.append(DieAssistantTrimProfile[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
DieAssistantTrimProfileList.erase(DieAssistantTrimProfile obj)
Erases the object from the list, but does not delete the object.
|
void |
DieAssistantTrimProfileList.erase(DieAssistantTrimProfile obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
DieAssistantTrimProfileList.findIndex(DieAssistantTrimProfile obj)
Finds the index where the input object appears.
|
void |
DieAssistantTrimProfileList.insert(int location,
DieAssistantTrimProfile object)
Inserts an object at the specified location
License requirements: None. |
void |
DieAssistantTrimProfileList.setContents(DieAssistantTrimProfile[] objects)
Sets the contents of the entire list.
|
void |
DieAssistantTrimProfileList.swap(DieAssistantTrimProfile object1,
DieAssistantTrimProfile object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.