Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.EDGE_ANGLE_END
Change the angle of the end edge of a planar face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.EDGE_ANGLE_START
Change the angle of the start edge of a planar face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.EDGE_EXTEND
Extend edge of a face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.EDGE_EXTEND_END
Extend end edge of a planar face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.EDGE_EXTEND_START
Extend start edge of a planar face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.EXTEND_UMAXIMUM
Extend the U Maximum edge of the anchor face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.EXTEND_UMINIMUM
Extend the U Minimum edge of the anchor face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.EXTEND_VMAXIMUM
Extend the V Maximum edge of the anchor face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.EXTEND_VMINIMUM
Extend the V Minimum edge of the anchor face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.FACE_CENTRAL_ANGLE
Change the central angle of a conical/cylindrical face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.FACE_RADIUS
Change the face radius of a conical/cylindrical face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.FACE_REVERSE_CONVEXITY
Reverse the convexity of a conical/cylindrical face.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.TRANSFORM
Transform body.
|
Modifier and Type | Method and Description |
---|---|
QuickBinderBuilder.EditTypes |
QuickBinderBuilder.editType()
Returns the type edit to be performed on the face or edge.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static QuickBinderBuilder.EditTypes |
QuickBinderBuilder.EditTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static QuickBinderBuilder.EditTypes[] |
QuickBinderBuilder.EditTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
QuickBinderBuilder.setEditType(QuickBinderBuilder.EditTypes type)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.