public static class QuickBinderBuilder.EditTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EDGE_ANGLE_END
Change the angle of the end edge of a planar face.
|
static int |
_EDGE_ANGLE_START
Change the angle of the start edge of a planar face.
|
static int |
_EDGE_EXTEND
Extend edge of a face.
|
static int |
_EDGE_EXTEND_END
Extend end edge of a planar face.
|
static int |
_EDGE_EXTEND_START
Extend start edge of a planar face.
|
static int |
_EXTEND_UMAXIMUM
Extend the U Maximum edge of the anchor face.
|
static int |
_EXTEND_UMINIMUM
Extend the U Minimum edge of the anchor face.
|
static int |
_EXTEND_VMAXIMUM
Extend the V Maximum edge of the anchor face.
|
static int |
_EXTEND_VMINIMUM
Extend the V Minimum edge of the anchor face.
|
static int |
_FACE_CENTRAL_ANGLE
Change the central angle of a conical/cylindrical face.
|
static int |
_FACE_RADIUS
Change the face radius of a conical/cylindrical face.
|
static int |
_FACE_REVERSE_CONVEXITY
Reverse the convexity of a conical/cylindrical face.
|
static int |
_TRANSFORM
Transform body.
|
static QuickBinderBuilder.EditTypes |
EDGE_ANGLE_END
Change the angle of the end edge of a planar face.
|
static QuickBinderBuilder.EditTypes |
EDGE_ANGLE_START
Change the angle of the start edge of a planar face.
|
static QuickBinderBuilder.EditTypes |
EDGE_EXTEND
Extend edge of a face.
|
static QuickBinderBuilder.EditTypes |
EDGE_EXTEND_END
Extend end edge of a planar face.
|
static QuickBinderBuilder.EditTypes |
EDGE_EXTEND_START
Extend start edge of a planar face.
|
static QuickBinderBuilder.EditTypes |
EXTEND_UMAXIMUM
Extend the U Maximum edge of the anchor face.
|
static QuickBinderBuilder.EditTypes |
EXTEND_UMINIMUM
Extend the U Minimum edge of the anchor face.
|
static QuickBinderBuilder.EditTypes |
EXTEND_VMAXIMUM
Extend the V Maximum edge of the anchor face.
|
static QuickBinderBuilder.EditTypes |
EXTEND_VMINIMUM
Extend the V Minimum edge of the anchor face.
|
static QuickBinderBuilder.EditTypes |
FACE_CENTRAL_ANGLE
Change the central angle of a conical/cylindrical face.
|
static QuickBinderBuilder.EditTypes |
FACE_RADIUS
Change the face radius of a conical/cylindrical face.
|
static QuickBinderBuilder.EditTypes |
FACE_REVERSE_CONVEXITY
Reverse the convexity of a conical/cylindrical face.
|
static QuickBinderBuilder.EditTypes |
TRANSFORM
Transform body.
|
Modifier and Type | Method and Description |
---|---|
static QuickBinderBuilder.EditTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static QuickBinderBuilder.EditTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static QuickBinderBuilder.EditTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final QuickBinderBuilder.EditTypes EDGE_EXTEND
public static final QuickBinderBuilder.EditTypes EDGE_EXTEND_START
public static final QuickBinderBuilder.EditTypes EDGE_EXTEND_END
public static final QuickBinderBuilder.EditTypes EDGE_ANGLE_START
public static final QuickBinderBuilder.EditTypes EDGE_ANGLE_END
public static final QuickBinderBuilder.EditTypes FACE_RADIUS
public static final QuickBinderBuilder.EditTypes FACE_CENTRAL_ANGLE
public static final QuickBinderBuilder.EditTypes FACE_REVERSE_CONVEXITY
public static final QuickBinderBuilder.EditTypes TRANSFORM
public static final QuickBinderBuilder.EditTypes EXTEND_UMINIMUM
public static final QuickBinderBuilder.EditTypes EXTEND_UMAXIMUM
public static final QuickBinderBuilder.EditTypes EXTEND_VMINIMUM
public static final QuickBinderBuilder.EditTypes EXTEND_VMAXIMUM
public static final int _EDGE_EXTEND
public static final int _EDGE_EXTEND_START
public static final int _EDGE_EXTEND_END
public static final int _EDGE_ANGLE_START
public static final int _EDGE_ANGLE_END
public static final int _FACE_RADIUS
public static final int _FACE_CENTRAL_ANGLE
public static final int _FACE_REVERSE_CONVEXITY
public static final int _TRANSFORM
public static final int _EXTEND_UMINIMUM
public static final int _EXTEND_UMAXIMUM
public static final int _EXTEND_VMINIMUM
public static final int _EXTEND_VMAXIMUM
public static QuickBinderBuilder.EditTypes valueOf(int value)
public static QuickBinderBuilder.EditTypes valueOf(String name)
public static QuickBinderBuilder.EditTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.