Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static TrimLineDevelopmentBuilder.SmoothingName |
TrimLineDevelopmentBuilder.SmoothingName.CUBIC
Cubic approximation
|
static TrimLineDevelopmentBuilder.SmoothingName |
TrimLineDevelopmentBuilder.SmoothingName.LINEAR
Linear (no smoothing)
|
static TrimLineDevelopmentBuilder.SmoothingName |
TrimLineDevelopmentBuilder.SmoothingName.QUINTIC
Quintic approximation
|
Modifier and Type | Method and Description |
---|---|
TrimLineDevelopmentBuilder.SmoothingName |
TrimLineDevelopmentBuilder.smoothing()
Returns the curve smoothing method - linear (none), cubic or quintic
License requirements: None. |
static TrimLineDevelopmentBuilder.SmoothingName |
TrimLineDevelopmentBuilder.SmoothingName.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimLineDevelopmentBuilder.SmoothingName |
TrimLineDevelopmentBuilder.SmoothingName.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimLineDevelopmentBuilder.SmoothingName[] |
TrimLineDevelopmentBuilder.SmoothingName.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimLineDevelopmentBuilder.setSmoothing(TrimLineDevelopmentBuilder.SmoothingName smoothing)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.