Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static FlangeTaskBuilder.SpringbackTypes |
FlangeTaskBuilder.SpringbackTypes.CONSTANT
Constant
|
static FlangeTaskBuilder.SpringbackTypes |
FlangeTaskBuilder.SpringbackTypes.LAW
Law Controlled
|
Modifier and Type | Method and Description |
---|---|
FlangeTaskBuilder.SpringbackTypes |
FlangeTaskBuilder.springbackType()
Returns the springback type of the flange task
License requirements: die_engineering ("DIE ENGINEERING") . |
static FlangeTaskBuilder.SpringbackTypes |
FlangeTaskBuilder.SpringbackTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeTaskBuilder.SpringbackTypes |
FlangeTaskBuilder.SpringbackTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeTaskBuilder.SpringbackTypes[] |
FlangeTaskBuilder.SpringbackTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlangeTaskBuilder.setSpringbackType(FlangeTaskBuilder.SpringbackTypes springbackType)
Sets the springback type of the flange task
License requirements: die_engineering ("DIE ENGINEERING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.