Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static OutputCurvesBuilder.TrimCurveCreateTypes |
OutputCurvesBuilder.TrimCurveCreateTypes.SECTION
Section.
|
static OutputCurvesBuilder.TrimCurveCreateTypes |
OutputCurvesBuilder.TrimCurveCreateTypes.SURFACE
Surface.
|
Modifier and Type | Method and Description |
---|---|
OutputCurvesBuilder.TrimCurveCreateTypes |
OutputCurvesBuilder.trimCurveCreateType()
Returns the trim curve creation type
License requirements: die_engineering ("DIE ENGINEERING") . |
static OutputCurvesBuilder.TrimCurveCreateTypes |
OutputCurvesBuilder.TrimCurveCreateTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OutputCurvesBuilder.TrimCurveCreateTypes |
OutputCurvesBuilder.TrimCurveCreateTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OutputCurvesBuilder.TrimCurveCreateTypes[] |
OutputCurvesBuilder.TrimCurveCreateTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OutputCurvesBuilder.setTrimCurveCreateType(OutputCurvesBuilder.TrimCurveCreateTypes trimCurveType)
Sets the trim curve creation type
License requirements: die_engineering ("DIE ENGINEERING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.