Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static WearPlateLocParentBuilder.PositionType |
WearPlateLocParentBuilder.PositionType.BOTH
Position locator on both sides of the wear plate.
|
static WearPlateLocParentBuilder.PositionType |
WearPlateLocParentBuilder.PositionType.LEFT
Position locator to the left of the wear plate.
|
static WearPlateLocParentBuilder.PositionType |
WearPlateLocParentBuilder.PositionType.NEITHER
No locators.
|
static WearPlateLocParentBuilder.PositionType |
WearPlateLocParentBuilder.PositionType.RIGHT
Position locator to the right of the wear plate.
|
Modifier and Type | Method and Description |
---|---|
WearPlateLocParentBuilder.PositionType |
WearPlateLocParentBuilder.locatorPosition()
Returns the locator position of die wear plate and locators
License requirements: ug_die_design ("Die Design") . |
static WearPlateLocParentBuilder.PositionType |
WearPlateLocParentBuilder.PositionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WearPlateLocParentBuilder.PositionType |
WearPlateLocParentBuilder.PositionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WearPlateLocParentBuilder.PositionType[] |
WearPlateLocParentBuilder.PositionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WearPlateLocParentBuilder.setLocatorPosition(WearPlateLocParentBuilder.PositionType position)
Sets the locator position of die wear plate and locators
License requirements: ug_die_design ("Die Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.