Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DiePlaneBuilder.PlaneType |
DiePlaneBuilder.PlaneType.COORDINATE_SYSTEM
Define a coordinate system to specify the plane.
|
static DiePlaneBuilder.PlaneType |
DiePlaneBuilder.PlaneType.PLANE
Define the plane to be used.
|
static DiePlaneBuilder.PlaneType |
DiePlaneBuilder.PlaneType.SELECTION
Select the plane to be used.
|
Modifier and Type | Method and Description |
---|---|
DiePlaneBuilder.PlaneType |
DiePlaneBuilder.inputType()
Returns the type of input that defined the plane
License requirements: None. |
static DiePlaneBuilder.PlaneType |
DiePlaneBuilder.PlaneType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DiePlaneBuilder.PlaneType |
DiePlaneBuilder.PlaneType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DiePlaneBuilder.PlaneType[] |
DiePlaneBuilder.PlaneType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DiePlaneBuilder.setInputType(DiePlaneBuilder.PlaneType inputType)
License requirements: ug_die_design ("Die Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.