public interface DieBooleanBuilder extends TaggedObject, IComponentBuilder
DieBooleanBuilder
. This class is a helper to other
Die Design features that identify specific booleans in their dialogs, such as the Die Shoe
feature.
DieCollection.createDieBoolean()
Modifier and Type | Interface and Description |
---|---|
static class |
DieBooleanBuilder.BooleanType
boolean type to apply to the selected solids
|
Modifier and Type | Method and Description |
---|---|
DieBooleanBuilder.BooleanType |
booleanOptions()
Returns the boolean option to apply to the list of selected solids
License requirements: None. |
SelectNXObjectList |
selectBodies()
Returns the bodies to be booleaned to the main feature body
License requirements: None. |
void |
setBooleanOptions(DieBooleanBuilder.BooleanType booleanOptions)
License requirements: ug_die_design ("Die Design") . |
printTestData, printTestData, tag, tagValue
validate
DieBooleanBuilder.BooleanType booleanOptions() throws NXException, RemoteException
NXException
RemoteException
void setBooleanOptions(DieBooleanBuilder.BooleanType booleanOptions) throws NXException, RemoteException
booleanOptions
- NXException
RemoteException
SelectNXObjectList selectBodies() throws NXException, RemoteException
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.