Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static PierceTaskBuilder.CenterPointOptionTypes |
PierceTaskBuilder.CenterPointOptionTypes.BOTH
Center points output in both die and product position
|
static PierceTaskBuilder.CenterPointOptionTypes |
PierceTaskBuilder.CenterPointOptionTypes.DIE
Center points output in die position
|
static PierceTaskBuilder.CenterPointOptionTypes |
PierceTaskBuilder.CenterPointOptionTypes.NONE
No center points output
|
static PierceTaskBuilder.CenterPointOptionTypes |
PierceTaskBuilder.CenterPointOptionTypes.PRODUCT
Center points output in product position
|
Modifier and Type | Method and Description |
---|---|
PierceTaskBuilder.CenterPointOptionTypes |
PierceTaskBuilder.centerPointOption()
Returns the center point output option of the pierce task
License requirements: die_engineering ("DIE ENGINEERING") . |
static PierceTaskBuilder.CenterPointOptionTypes |
PierceTaskBuilder.CenterPointOptionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PierceTaskBuilder.CenterPointOptionTypes |
PierceTaskBuilder.CenterPointOptionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PierceTaskBuilder.CenterPointOptionTypes[] |
PierceTaskBuilder.CenterPointOptionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PierceTaskBuilder.setCenterPointOption(PierceTaskBuilder.CenterPointOptionTypes centerPointOption)
Sets the center point output option of the pierce task
License requirements: die_engineering ("DIE ENGINEERING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.