Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DieLocationBuilder.LocationType |
DieLocationBuilder.LocationType.NEW_COORDINATE_SYSTEM
Define a coordinate system to specify the location.
|
static DieLocationBuilder.LocationType |
DieLocationBuilder.LocationType.NEW_PLANE
Define a plane to specify the location.
|
static DieLocationBuilder.LocationType |
DieLocationBuilder.LocationType.NEW_POINT
Define the point to be used.
|
static DieLocationBuilder.LocationType |
DieLocationBuilder.LocationType.NEW_VECTOR
Define a vector to specify the location.
|
static DieLocationBuilder.LocationType |
DieLocationBuilder.LocationType.SELECT_LOCATION
Select the point to be used.
|
Modifier and Type | Method and Description |
---|---|
DieLocationBuilder.LocationType |
DieLocationBuilder.inputType()
Returns the type of source that defined the location
License requirements: None. |
static DieLocationBuilder.LocationType |
DieLocationBuilder.LocationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieLocationBuilder.LocationType |
DieLocationBuilder.LocationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieLocationBuilder.LocationType[] |
DieLocationBuilder.LocationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieLocationBuilder.setInputType(DieLocationBuilder.LocationType inputType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.