Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static AddendumSectionBuilder.SegmentType |
AddendumSectionBuilder.SegmentType.DIE_PUNCH
Update die punch segment.
|
static AddendumSectionBuilder.SegmentType |
AddendumSectionBuilder.SegmentType.DIE_REVERSE
Update die reverse segment.
|
static AddendumSectionBuilder.SegmentType |
AddendumSectionBuilder.SegmentType.FIRST_STRETCH_WALL
Update first stretch wall segment.
|
static AddendumSectionBuilder.SegmentType |
AddendumSectionBuilder.SegmentType.FLAT_TO_BEAD
Update flat to bead segment.
|
static AddendumSectionBuilder.SegmentType |
AddendumSectionBuilder.SegmentType.PLUS
Update plus segment.
|
static AddendumSectionBuilder.SegmentType |
AddendumSectionBuilder.SegmentType.PUNCH
Update punch segment.
|
static AddendumSectionBuilder.SegmentType |
AddendumSectionBuilder.SegmentType.REVERSE
Update reverse segment.
|
static AddendumSectionBuilder.SegmentType |
AddendumSectionBuilder.SegmentType.SECOND_STRETCH_WALL
Update second stretch wall segment.
|
static AddendumSectionBuilder.SegmentType |
AddendumSectionBuilder.SegmentType.TRIM_LEDGE
Update trim ledge segment.
|
Modifier and Type | Method and Description |
---|---|
static AddendumSectionBuilder.SegmentType |
AddendumSectionBuilder.SegmentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AddendumSectionBuilder.SegmentType |
AddendumSectionBuilder.SegmentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AddendumSectionBuilder.SegmentType[] |
AddendumSectionBuilder.SegmentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AddendumSectionBuilder.lockSegment(Curve section,
AddendumSectionBuilder.SegmentType segment,
AddendumSectionBuilder.SegmentParameterType type)
Lock a segment parameter value.
|
void |
AddendumSectionBuilder.unlockSegment(Curve section,
AddendumSectionBuilder.SegmentType segment,
AddendumSectionBuilder.SegmentParameterType type)
Unlock a segment parameter value.
|
double |
AddendumSectionBuilder.updateSegment(boolean temporary,
Curve section,
AddendumSectionBuilder.SegmentType segment,
double lengthRadius,
double angle)
Updates length or angle value of a segment.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.