Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DrawBeadTaperBuilder.TaperTypes |
DrawBeadTaperBuilder.TaperTypes.POINT
Use the spherical method, but the radius is defined by a point location and distance to the end of the centerline.
|
static DrawBeadTaperBuilder.TaperTypes |
DrawBeadTaperBuilder.TaperTypes.SPHERICAL
Create a spherical end based on a radius.
|
static DrawBeadTaperBuilder.TaperTypes |
DrawBeadTaperBuilder.TaperTypes.WASHOUT
Create a slope based on the height and length desired.
|
Modifier and Type | Method and Description |
---|---|
DrawBeadTaperBuilder.TaperTypes |
DrawBeadTaperBuilder.taperType()
Returns the method to apply for defining the taper.
|
static DrawBeadTaperBuilder.TaperTypes |
DrawBeadTaperBuilder.TaperTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadTaperBuilder.TaperTypes |
DrawBeadTaperBuilder.TaperTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadTaperBuilder.TaperTypes[] |
DrawBeadTaperBuilder.TaperTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawBeadTaperBuilder.setTaperType(DrawBeadTaperBuilder.TaperTypes taperType)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.