public static class DrawBeadTaperBuilder.TaperTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_POINT
Use the spherical method, but the radius is defined by a point location and distance to the end of the centerline.
|
static int |
_SPHERICAL
Create a spherical end based on a radius.
|
static int |
_WASHOUT
Create a slope based on the height and length desired.
|
static DrawBeadTaperBuilder.TaperTypes |
POINT
Use the spherical method, but the radius is defined by a point location and distance to the end of the centerline.
|
static DrawBeadTaperBuilder.TaperTypes |
SPHERICAL
Create a spherical end based on a radius.
|
static DrawBeadTaperBuilder.TaperTypes |
WASHOUT
Create a slope based on the height and length desired.
|
Modifier and Type | Method and Description |
---|---|
static DrawBeadTaperBuilder.TaperTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadTaperBuilder.TaperTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadTaperBuilder.TaperTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final DrawBeadTaperBuilder.TaperTypes SPHERICAL
public static final DrawBeadTaperBuilder.TaperTypes WASHOUT
public static final DrawBeadTaperBuilder.TaperTypes POINT
public static final int _SPHERICAL
public static final int _WASHOUT
public static final int _POINT
public static DrawBeadTaperBuilder.TaperTypes valueOf(int value)
public static DrawBeadTaperBuilder.TaperTypes valueOf(String name)
public static DrawBeadTaperBuilder.TaperTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.