Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static FingerClearanceNotchBuilder.Types |
FingerClearanceNotchBuilder.Types.FACE
Build from either a single face or a set of connected faces.
|
static FingerClearanceNotchBuilder.Types |
FingerClearanceNotchBuilder.Types.SECTION
Build from an open section profile.
|
static FingerClearanceNotchBuilder.Types |
FingerClearanceNotchBuilder.Types.SHEET_BODY
Build from either a sheet body or a solid body.
|
Modifier and Type | Method and Description |
---|---|
FingerClearanceNotchBuilder.Types |
FingerClearanceNotchBuilder.type()
Returns the indicator specifying the type of input data that defines how to build the notch.
|
static FingerClearanceNotchBuilder.Types |
FingerClearanceNotchBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FingerClearanceNotchBuilder.Types |
FingerClearanceNotchBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FingerClearanceNotchBuilder.Types[] |
FingerClearanceNotchBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FingerClearanceNotchBuilder.setType(FingerClearanceNotchBuilder.Types type)
License requirements: ug_die_design ("Die Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.