Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Method and Description |
---|---|
DieLocationBuilder |
HeelpostBuilder.center()
Returns the location (center) for the heelpost
License requirements: None. |
DieLocationBuilder |
DieCollection.createDieLocation()
Creates a
DieLocationBuilder . |
DieLocationBuilder |
MachineReliefBuilder.end()
Returns the location for the end of the segment definition.
|
DieLocationBuilder |
DrawBeadBuilder.endPoint()
Returns the point location defining the end of the centerline.
|
DieLocationBuilder |
DieLocationBuilderList.findItem(int index)
Returns the object at the input index.
|
DieLocationBuilder[] |
DieLocationBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
DieLocationBuilder |
MachineReliefBuilder.start()
Returns the location for the start of the segment definition.
|
DieLocationBuilder |
DrawBeadBuilder.startPoint()
Returns the point location defining the start of the centerline.
|
Modifier and Type | Method and Description |
---|---|
void |
DieLocationBuilderList.append(DieLocationBuilder object)
Appends an object to the list
License requirements: None. |
void |
DieLocationBuilderList.append(DieLocationBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
DieLocationBuilderList.erase(DieLocationBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
DieLocationBuilderList.erase(DieLocationBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
DieLocationBuilderList.findIndex(DieLocationBuilder obj)
Finds the index where the input object appears.
|
void |
DieLocationBuilderList.insert(int location,
DieLocationBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
DieLocationBuilderList.setContents(DieLocationBuilder[] objects)
Sets the contents of the entire list.
|
void |
DieLocationBuilderList.swap(DieLocationBuilder object1,
DieLocationBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.