public interface MachineReliefBuilder extends FeatureBuilder
MachineRelief
feature. The builder may generate a Cam Definition, Machine Relief, or Wall Thickness.
DieCollection.createMachineReliefBuilder(nxopen.die.MachineRelief)
Property | Value |
---|---|
BaseOffset.Value | 0 (millimeters part), 0 (inches part) |
BeltFaceThickness.Value | 20 (millimeters part), 0.8 (inches part) |
End.InputType | SelectLocation |
JogWall | 0 |
MainProfileType | Exterior |
Offset.Value | 20 (millimeters part), 0.8 (inches part) |
ProfileOffset.Value | 30 (millimeters part), 1.2 (inches part) |
Relief.Value | 20 (millimeters part), 0.8 (inches part) |
ReliefOffset.Value | 5 (millimeters part), 0.2 (inches part) |
TopOffset.Value | 1000 (millimeters part), 40 (inches part) |
TrimOffset.Value | 5 (millimeters part), 0.2 (inches part) |
TrimSheetOffset.Value | 0 (millimeters part), 0 (inches part) |
TrimSheetType | Sheet |
WallOffset.Value | 10 (millimeters part), 0.4 (inches part) |
WallThickness.Value | 45 (millimeters part), 1.8 (inches part) |
Modifier and Type | Interface and Description |
---|---|
static class |
MachineReliefBuilder.MainProfileTypes
Specifies that the profile is for an exterior or interior profile.
|
static class |
MachineReliefBuilder.TrimSheetTypes
Specifies what the trimming surface is defined by.
|
static class |
MachineReliefBuilder.Types
Identifies the type of structure to be added, or subtracted, to the casting.
|
Modifier and Type | Method and Description |
---|---|
double |
angleTolerance()
Returns the angle tolerance.
|
Expression |
baseOffset()
Returns the expression containing the offset value to apply to the base definition before trimming the base of the tool solids.
|
DiePlaneBuilder |
baseOrientation()
Returns the base orientation of the target solid.
|
DieAttributesBuilder |
beltAttributes()
Returns the attribute title, value and face color to apply to the belt faces.
|
Expression |
beltFaceThickness()
Returns the expression containing the value to apply for the belt face on the cam definition.
|
DieDirectionBuilder |
camDirection()
Returns the direction of the cam for trimming.
|
double |
distanceTolerance()
Returns the distance tolerance.
|
DieLocationBuilder |
end()
Returns the location for the end of the segment definition.
|
Section |
insideWallProfile()
Returns the wall profile defining the inside of the main wall used for the cam definition.
|
boolean |
jogWall()
Returns the indicator defining if the wall should be jogged (or changed) to accommodate the cam definition.
|
Section |
mainProfile()
Returns the primary profile for the machine relief casting.
|
MachineReliefBuilder.MainProfileTypes |
mainProfileType()
Returns the value specifying the main profile for the Thicken operation.
|
Expression |
offset()
Returns the expression containing the value to apply for the thicken operation to create the tool solid.
|
Expression |
profileOffset()
Returns the expression containing the value to apply to the profile to create the primary head solid for the cam definition.
|
Expression |
relief()
Returns the expression containing the value to apply for the machine relief operation to create the tool solid.
|
Expression |
reliefOffset()
Returns the expression containing the value of the relief around the primary head solid for the cam definition if a wall is created.
|
void |
setAngleTolerance(double angleTolerance)
License requirements: ug_die_design ("Die Design") . |
void |
setDistanceTolerance(double distanceTolerance)
License requirements: ug_die_design ("Die Design") . |
void |
setJogWall(boolean jogWall)
License requirements: ug_die_design ("Die Design") . |
void |
setMainProfileType(MachineReliefBuilder.MainProfileTypes mainProfileType)
License requirements: ug_die_design ("Die Design") . |
void |
setSwitchTrimSide(boolean switchTrimSide)
License requirements: ug_die_design ("Die Design") . |
void |
setTrimSheetType(MachineReliefBuilder.TrimSheetTypes trimSheetType)
License requirements: ug_die_design ("Die Design") . |
void |
setType(MachineReliefBuilder.Types type)
License requirements: ug_die_design ("Die Design") . |
DieLocationBuilder |
start()
Returns the location for the start of the segment definition.
|
boolean |
switchTrimSide()
Returns the indicator if the trim side should be switched from the default for the sheet metal.
|
SelectBody |
target()
Returns the target solid to add or subtract material too.
|
Expression |
topOffset()
Returns the expression containing the offset value from the base to define the top extent of the internal builds.
|
Expression |
trimOffset()
Returns the expression containing the clearance value to apply at the start and the end of the cam definition to define the primary head solid.
|
SelectBody |
trimSheet()
Returns the sheet body selection for the trim sheet.
|
ScCollector |
trimSheetFace()
Returns the face selections to define the trim sheet.
|
Expression |
trimSheetOffset()
Returns the expression containing the offset value to apply to the trim sheet to construct the tool solids.
|
MachineReliefBuilder.TrimSheetTypes |
trimSheetType()
Returns the indicator for how the trim sheet is specified.
|
MachineReliefBuilder.Types |
type()
Returns the value defining the type of build to perform for this tool.
|
Expression |
wallOffset()
Returns the expression containing the offset to apply to the wall to create the wall area for the cam definition.
|
Expression |
wallThickness()
Returns the expression containing the thickness value of the wall for the cam definition.
|
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectBody target() throws NXException, RemoteException
NXException
RemoteException
DiePlaneBuilder baseOrientation() throws NXException, RemoteException
NXException
RemoteException
Expression baseOffset() throws NXException, RemoteException
NXException
RemoteException
Expression topOffset() throws NXException, RemoteException
NXException
RemoteException
MachineReliefBuilder.MainProfileTypes mainProfileType() throws NXException, RemoteException
MachineReliefBuilder.Types.THICKEN
.
NXException
RemoteException
void setMainProfileType(MachineReliefBuilder.MainProfileTypes mainProfileType) throws NXException, RemoteException
mainProfileType
- NXException
RemoteException
Section mainProfile() throws NXException, RemoteException
NXException
RemoteException
boolean switchTrimSide() throws NXException, RemoteException
NXException
RemoteException
void setSwitchTrimSide(boolean switchTrimSide) throws NXException, RemoteException
switchTrimSide
- NXException
RemoteException
DieLocationBuilder start() throws NXException, RemoteException
NXException
RemoteException
DieLocationBuilder end() throws NXException, RemoteException
NXException
RemoteException
DieDirectionBuilder camDirection() throws NXException, RemoteException
MachineReliefBuilder.Types.CAM
or MachineReliefBuilder.Types.RELIEF
.
NXException
RemoteException
MachineReliefBuilder.TrimSheetTypes trimSheetType() throws NXException, RemoteException
NXException
RemoteException
void setTrimSheetType(MachineReliefBuilder.TrimSheetTypes trimSheetType) throws NXException, RemoteException
trimSheetType
- NXException
RemoteException
SelectBody trimSheet() throws NXException, RemoteException
NXException
RemoteException
ScCollector trimSheetFace() throws NXException, RemoteException
NXException
RemoteException
Expression trimSheetOffset() throws NXException, RemoteException
MachineReliefBuilder.Types.RELIEF
or MachineReliefBuilder.Types.THICKEN
.
NXException
RemoteException
Section insideWallProfile() throws NXException, RemoteException
MachineReliefBuilder.Types.CAM
.
NXException
RemoteException
Expression offset() throws NXException, RemoteException
MachineReliefBuilder.Types.RELIEF
or MachineReliefBuilder.Types.THICKEN
.
NXException
RemoteException
Expression relief() throws NXException, RemoteException
MachineReliefBuilder.Types.RELIEF
or MachineReliefBuilder.Types.THICKEN
.
NXException
RemoteException
Expression beltFaceThickness() throws NXException, RemoteException
MachineReliefBuilder.Types.CAM
.
NXException
RemoteException
Expression profileOffset() throws NXException, RemoteException
MachineReliefBuilder.Types.CAM
.
NXException
RemoteException
Expression reliefOffset() throws NXException, RemoteException
MachineReliefBuilder.Types.CAM
.
NXException
RemoteException
Expression trimOffset() throws NXException, RemoteException
MachineReliefBuilder.Types.CAM
.
NXException
RemoteException
Expression wallOffset() throws NXException, RemoteException
MachineReliefBuilder.Types.CAM
.
NXException
RemoteException
Expression wallThickness() throws NXException, RemoteException
MachineReliefBuilder.Types.CAM
.
NXException
RemoteException
boolean jogWall() throws NXException, RemoteException
NXException
RemoteException
void setJogWall(boolean jogWall) throws NXException, RemoteException
jogWall
- NXException
RemoteException
DieAttributesBuilder beltAttributes() throws NXException, RemoteException
NXException
RemoteException
double distanceTolerance() throws NXException, RemoteException
NXException
RemoteException
void setDistanceTolerance(double distanceTolerance) throws NXException, RemoteException
distanceTolerance
- NXException
RemoteException
double angleTolerance() throws NXException, RemoteException
NXException
RemoteException
void setAngleTolerance(double angleTolerance) throws NXException, RemoteException
angleTolerance
- NXException
RemoteException
MachineReliefBuilder.Types type() throws NXException, RemoteException
NXException
RemoteException
void setType(MachineReliefBuilder.Types type) throws NXException, RemoteException
type
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.