public static class MachineReliefBuilder.TrimSheetTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FACE
Trimming surface is a face, or faces to be sewed together.
|
static int |
_SHEET
Trimming surface is a sheet body.
|
static MachineReliefBuilder.TrimSheetTypes |
FACE
Trimming surface is a face, or faces to be sewed together.
|
static MachineReliefBuilder.TrimSheetTypes |
SHEET
Trimming surface is a sheet body.
|
Modifier and Type | Method and Description |
---|---|
static MachineReliefBuilder.TrimSheetTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MachineReliefBuilder.TrimSheetTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MachineReliefBuilder.TrimSheetTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final MachineReliefBuilder.TrimSheetTypes SHEET
public static final MachineReliefBuilder.TrimSheetTypes FACE
public static final int _SHEET
public static final int _FACE
public static MachineReliefBuilder.TrimSheetTypes valueOf(int value)
public static MachineReliefBuilder.TrimSheetTypes valueOf(String name)
public static MachineReliefBuilder.TrimSheetTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.