Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DrawBeadBuilder.ProjectionDirectionTypes |
DrawBeadBuilder.ProjectionDirectionTypes.DRAW_DIRECTION
Project the centerline along the draw direction vector.
|
static DrawBeadBuilder.ProjectionDirectionTypes |
DrawBeadBuilder.ProjectionDirectionTypes.NORMAL_TO_PLACEMENT_FACE
Project the centerline along the placement face normal.
|
Modifier and Type | Method and Description |
---|---|
DrawBeadBuilder.ProjectionDirectionTypes |
DrawBeadBuilder.centerlineProjection()
Returns the projection method to apply to the centerline to place it on the sewn faces.
|
static DrawBeadBuilder.ProjectionDirectionTypes |
DrawBeadBuilder.ProjectionDirectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.ProjectionDirectionTypes |
DrawBeadBuilder.ProjectionDirectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.ProjectionDirectionTypes[] |
DrawBeadBuilder.ProjectionDirectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawBeadBuilder.setCenterlineProjection(DrawBeadBuilder.ProjectionDirectionTypes centerlineProjection)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.