Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static AddendumSectionBuilder.SegmentParameterType |
AddendumSectionBuilder.SegmentParameterType.ANGLE
The angle parameter of a straight segment.
|
static AddendumSectionBuilder.SegmentParameterType |
AddendumSectionBuilder.SegmentParameterType.ARC_LENGTH
The arc length parameter of an arc segment.
|
static AddendumSectionBuilder.SegmentParameterType |
AddendumSectionBuilder.SegmentParameterType.LENGTH
The length parameter of a straight segment.
|
static AddendumSectionBuilder.SegmentParameterType |
AddendumSectionBuilder.SegmentParameterType.RADIUS
The radius parameter of an arc segment.
|
Modifier and Type | Method and Description |
---|---|
static AddendumSectionBuilder.SegmentParameterType |
AddendumSectionBuilder.SegmentParameterType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AddendumSectionBuilder.SegmentParameterType |
AddendumSectionBuilder.SegmentParameterType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AddendumSectionBuilder.SegmentParameterType[] |
AddendumSectionBuilder.SegmentParameterType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AddendumSectionBuilder.lockSegment(Curve section,
AddendumSectionBuilder.SegmentType segment,
AddendumSectionBuilder.SegmentParameterType type)
Lock a segment parameter value.
|
void |
AddendumSectionBuilder.unlockSegment(Curve section,
AddendumSectionBuilder.SegmentType segment,
AddendumSectionBuilder.SegmentParameterType type)
Unlock a segment parameter value.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.