Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static FlangeTaskBuilder.PierceTypes |
FlangeTaskBuilder.PierceTypes.CRITICAL
Use Critical tolerance.
|
static FlangeTaskBuilder.PierceTypes |
FlangeTaskBuilder.PierceTypes.GAGE
Use Gage tolerance.
|
static FlangeTaskBuilder.PierceTypes |
FlangeTaskBuilder.PierceTypes.STANDARD
Use Standard tolerance.
|
Modifier and Type | Method and Description |
---|---|
FlangeTaskBuilder.PierceTypes |
FlangeTaskBuilder.pierceType()
Returns the pierce type of the flange task
License requirements: die_engineering ("DIE ENGINEERING") . |
static FlangeTaskBuilder.PierceTypes |
FlangeTaskBuilder.PierceTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeTaskBuilder.PierceTypes |
FlangeTaskBuilder.PierceTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeTaskBuilder.PierceTypes[] |
FlangeTaskBuilder.PierceTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlangeTaskBuilder.setPierceType(FlangeTaskBuilder.PierceTypes pierceType)
Sets the pierce type of the flange task
License requirements: die_engineering ("DIE ENGINEERING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.