Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static TrimLineDevelopmentBuilder.MeshElement |
TrimLineDevelopmentBuilder.MeshElement.QUADRATE
Generate 2D quadrate mesh element
|
static TrimLineDevelopmentBuilder.MeshElement |
TrimLineDevelopmentBuilder.MeshElement.TRIANGLE
Generate 2D triangle mesh element
|
Modifier and Type | Method and Description |
---|---|
TrimLineDevelopmentBuilder.MeshElement |
TrimLineDevelopmentBuilder.meshElementType()
Returns the 2-D mesh element type, either triangle or quadrate element.
|
static TrimLineDevelopmentBuilder.MeshElement |
TrimLineDevelopmentBuilder.MeshElement.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimLineDevelopmentBuilder.MeshElement |
TrimLineDevelopmentBuilder.MeshElement.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimLineDevelopmentBuilder.MeshElement[] |
TrimLineDevelopmentBuilder.MeshElement.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimLineDevelopmentBuilder.setMeshElementType(TrimLineDevelopmentBuilder.MeshElement meshElementType)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.