Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Method and Description |
---|---|
DieAssistantFlangeProfile |
DieAssistantFlangeProfileList.findItem(int index)
Returns the object at the input index.
|
DieAssistantFlangeProfile[] |
DieAssistantFlangeProfileList.getContents()
Gets the contents of the entire list
License requirements: None. |
DieAssistantFlangeProfile |
TrimFlangeDieAssistantBuilder.newFlangeProfile()
Creates a new flange profile item in the set
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DieAssistantFlangeProfileList.append(DieAssistantFlangeProfile object)
Appends an object to the list
License requirements: None. |
void |
DieAssistantFlangeProfileList.append(DieAssistantFlangeProfile[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
DieAssistantFlangeProfileList.erase(DieAssistantFlangeProfile obj)
Erases the object from the list, but does not delete the object.
|
void |
DieAssistantFlangeProfileList.erase(DieAssistantFlangeProfile obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
DieAssistantFlangeProfileList.findIndex(DieAssistantFlangeProfile obj)
Finds the index where the input object appears.
|
void |
DieAssistantFlangeProfileList.insert(int location,
DieAssistantFlangeProfile object)
Inserts an object at the specified location
License requirements: None. |
void |
DieAssistantFlangeProfileList.setContents(DieAssistantFlangeProfile[] objects)
Sets the contents of the entire list.
|
void |
DieAssistantFlangeProfileList.swap(DieAssistantFlangeProfile object1,
DieAssistantFlangeProfile object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.