Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DrawBeadBuilder.FemaleWidthTypes |
DrawBeadBuilder.FemaleWidthTypes.CONSTANT
The female width is a user specified constant.
|
static DrawBeadBuilder.FemaleWidthTypes |
DrawBeadBuilder.FemaleWidthTypes.DERIVED
The female width is derived from the male (Male Width + 2(Sheet Metal Thickness + Clearance)).
|
Modifier and Type | Method and Description |
---|---|
DrawBeadBuilder.FemaleWidthTypes |
DrawBeadBuilder.femaleWidthType()
Returns the method used to calculate the female width.
|
static DrawBeadBuilder.FemaleWidthTypes |
DrawBeadBuilder.FemaleWidthTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.FemaleWidthTypes |
DrawBeadBuilder.FemaleWidthTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.FemaleWidthTypes[] |
DrawBeadBuilder.FemaleWidthTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawBeadBuilder.setFemaleWidthType(DrawBeadBuilder.FemaleWidthTypes femaleWidthType)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.