Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static TrimLineDevelopmentBuilder.Convergency |
TrimLineDevelopmentBuilder.Convergency.HIGH
Onestep solver convergency level is high
|
static TrimLineDevelopmentBuilder.Convergency |
TrimLineDevelopmentBuilder.Convergency.LOW
Onestep solver convergency level is low
|
static TrimLineDevelopmentBuilder.Convergency |
TrimLineDevelopmentBuilder.Convergency.MEDIUM
Onestep solver convergency level is medium
|
Modifier and Type | Method and Description |
---|---|
TrimLineDevelopmentBuilder.Convergency |
TrimLineDevelopmentBuilder.solverConvergencyLevel()
Returns the convergency level of onestep solver.
|
static TrimLineDevelopmentBuilder.Convergency |
TrimLineDevelopmentBuilder.Convergency.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimLineDevelopmentBuilder.Convergency |
TrimLineDevelopmentBuilder.Convergency.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimLineDevelopmentBuilder.Convergency[] |
TrimLineDevelopmentBuilder.Convergency.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimLineDevelopmentBuilder.setSolverConvergencyLevel(TrimLineDevelopmentBuilder.Convergency solverConvergencyLevel)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.