Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static TrimTaskBuilder.MatchCutTypes |
TrimTaskBuilder.MatchCutTypes.AT_BOTH
At both start and end planes.
|
static TrimTaskBuilder.MatchCutTypes |
TrimTaskBuilder.MatchCutTypes.AT_END
At end plane only.
|
static TrimTaskBuilder.MatchCutTypes |
TrimTaskBuilder.MatchCutTypes.AT_START
At start plane only.
|
static TrimTaskBuilder.MatchCutTypes |
TrimTaskBuilder.MatchCutTypes.NONE
No match cut.
|
Modifier and Type | Method and Description |
---|---|
TrimTaskBuilder.MatchCutTypes |
TrimTaskBuilder.matchCutType()
Returns the match cut type of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
static TrimTaskBuilder.MatchCutTypes |
TrimTaskBuilder.MatchCutTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimTaskBuilder.MatchCutTypes |
TrimTaskBuilder.MatchCutTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimTaskBuilder.MatchCutTypes[] |
TrimTaskBuilder.MatchCutTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimTaskBuilder.setMatchCutType(TrimTaskBuilder.MatchCutTypes matchCutType)
Sets the match cut type of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.