NXOpen.Routing.AddFontBuilder |
Builder for creating an add font user interface dialogue |
NXOpen.Routing.Anchor |
A Routing Anchor defines a position in a Qualified Routing component part. |
NXOpen.Routing.AnchorCollection |
Represents a collection of NXOpen.Routing.Anchor objects. |
NXOpen.Routing.ArcSegment |
Represents a arc segment. |
NXOpen.Routing.ArcSegmentCollection |
Represents a collection of NXOpen.Routing.ArcSegment objects. |
NXOpen.Routing.AssemblyDefinition |
Represents a collection of NXOpen.Routing.SingleDevice objects that are used in an assembled product. |
NXOpen.Routing.AssignCornerBuilder |
Builder class for Assign Corner which creates corner |
NXOpen.Routing.AssignDiscontinuityBuilder |
the Builder to Assign Discontinuity for the stocks |
NXOpen.Routing.AssignPathBuilder |
Assigns path to a broken routing run |
NXOpen.Routing.AttributeHolder |
Represents a NXOpen.Routing.AttributeHolder |
NXOpen.Routing.AttributeMembersBuilder |
Creates attibutemembers builder object to add to the search criteria list used by FindByAttributesBuilder |
NXOpen.Routing.BendCorner |
Computes a fillet curve between two linear segments to form a smooth bend transition from one segment to another. |
NXOpen.Routing.BendCornerCollection |
Represents a collection of NXOpen.Routing.BendCorner objects. |
NXOpen.Routing.BranchPathNumberingBuilder |
Builder class for Branch Path Numbering. |
NXOpen.Routing.BuiltInPath |
The Routing BuiltInPath object stores a set of curves. |
NXOpen.Routing.BuiltInPathCollection |
Represents a collection of NXOpen.Routing.BuiltInPath objects. |
NXOpen.Routing.CharacteristicList |
Contains a list of characteristics. |
NXOpen.Routing.ClockPartBuilder |
Builder class for clock part object |
NXOpen.Routing.CompareRunsBuilder |
Represents a NXOpen.Routing.CompareRunsBuilder , used to compare runs in the work part to the ones in another part, or to runs defined in xml files gathered in a folder (native mode) or on an item revision (managed mode). |
NXOpen.Routing.ConnectPathBuilder |
Represents a NXOpen.Routing.ConnectPathBuilder . |
NXOpen.Routing.ConnectedCurvesBuilder |
Builder for creating automatically creating segments on end-to-end connected curves. |
NXOpen.Routing.ConnectivityDefinition |
The base class for various connection objects. |
NXOpen.Routing.ControlPoint |
Routing Control Points define a position in space, and are used to determine connections from segments to segments, and segments to ports. |
NXOpen.Routing.ControlPointCollection |
Represents a collection of NXOpen.Routing.ControlPoint objects. |
NXOpen.Routing.CopeCorner |
The cope corner is a corner that trims stocks at a junction. |
NXOpen.Routing.CopeCornerBuilder |
Builder class for Cope Corner object |
NXOpen.Routing.CopeCornerCollection |
Represents a collection of NXOpen.Routing.CopeCorner objects. |
NXOpen.Routing.Corner |
The Routing Corner is the abstract parent class of all other corner objects. |
NXOpen.Routing.CornerCollection |
Represents a collection of NXOpen.Routing.Corner objects. |
NXOpen.Routing.CornerTypeBuilder |
Contains setting for corner creation. |
NXOpen.Routing.CreateFabricationBuilder |
Builder class to fabricate subassembly from standard parts, path segments, stock, and other routing objects within the current routing assembly |
NXOpen.Routing.CrossSection |
A NXOpen.Routing.CrossSection defines a profile to sweep for NXOpen.Routing.Stock objects. |
NXOpen.Routing.CrossSectionCollection |
Represents a collection of NXOpen.Routing.CrossSection objects. |
NXOpen.Routing.DefineRunBuilder |
Builder Class for DefineRun Object |
NXOpen.Routing.DeleteFontsBuilder |
Represents a NXOpen.Routing.DeleteFontsBuilder |
NXOpen.Routing.DeleteGapsBuilder |
Represents a NXOpen.Routing.DeleteGapsBuilder |
NXOpen.Routing.DeleteObjectsBuilder |
Represents a NXOpen.Routing.DeleteObjectsBuilder |
NXOpen.Routing.DesignRule |
Represents NXOpen.Routing.DesignRule object |
NXOpen.Routing.DesignRuleCollection |
Represents a collection of NXOpen.Routing.DesignRule objects. |
NXOpen.Routing.DesignRuleManager |
Represents NXOpen.Routing.DesignRuleManager object |
NXOpen.Routing.DesignRuleOverride |
Represents Routing DesignRuleOverride object |
NXOpen.Routing.DesignRuleViolation |
Represents NXOpen.Routing.DesignRuleViolation object |
NXOpen.Routing.DesignRuleViolationCollection |
Represents a collection of NXOpen.Routing.DesignRuleViolation objects. |
NXOpen.Routing.DesignRuleViolationLocation |
Represents NXOpen.Routing.DesignRuleViolationLocation object |
NXOpen.Routing.DesignRuleViolationLocationCollection |
Represents a collection of NXOpen.Routing.DesignRuleViolationLocation objects. |
NXOpen.Routing.DesignRuleViolationViewer |
This class can be used to set the violation id, update text for overridding the violation and update the user name used to override the violation. |
NXOpen.Routing.DeviceRelationship |
Represents a relationship between NXOpen.Routing.SingleDevice objects. |
NXOpen.Routing.DiscontinuityCorner |
A discontinuity corner is a corner that forces Routing.Stock objects to split as they cover the segments attached to the discontinuity corner. |
NXOpen.Routing.DiscontinuityCornerCollection |
Represents a collection of NXOpen.Routing.DiscontinuityCorner objects. |
NXOpen.Routing.Division |
Represents NXOpen.Routing.Division |
NXOpen.Routing.DivisionsBuilder |
Represents a NXOpen.Routing.DivisionsBuilder |
NXOpen.Routing.DuctReinforcement |
Represents a Duct Reinforcement feature used for creating/editing reinforcements on the inside or outside of rectangular HVAC ducts. |
NXOpen.Routing.DuctReinforcementBuilder |
Builder for creating/editing duct reinforcements. |
NXOpen.Routing.DuctSizeCalculatorBuilder |
Builder to perform calculations of the duct which is to be used in the HVAC applications. |
NXOpen.Routing.EditBendAngleBuilder |
To create a new instance of this class, use NXOpen.Routing.RouteManager.CreateEditBendAngleBuilder |
NXOpen.Routing.EditCharacteristicsBuilder |
Builder to edit required and optional characteristics of Routing.Stock or Assemblies.Component as defined in the application view file. |
NXOpen.Routing.EditLineSegmentBuilder |
Builder for the “Edit Line Segment” operation. |
NXOpen.Routing.EditPlacePartBuilder |
To create a new instance of this class, use NXOpen.Routing.RouteManager.CreateEditPlacePartBuilder |
NXOpen.Routing.ElbowSnapSettings |
Helper object used the by NXOpen.Routing.LinearPathBuilder builder. |
NXOpen.Routing.ExtractPort |
Routing ExtractPort object is an extract of Port class |
NXOpen.Routing.FeaturePort |
NXOpen.Routing.FeaturePort is a NXOpen.Features.Feature associated |
NXOpen.Routing.Filler |
Represents a Filler |
NXOpen.Routing.FillerCollection |
Represents a collection of NXOpen.Routing.Stock objects. |
NXOpen.Routing.FillerStockBuilder |
Creates Filler stock on selected Segments. |
NXOpen.Routing.FindByAttributesBuilder |
Find runs/objects with specified attribute name and attribute value criteria, |
NXOpen.Routing.FittingOverstock |
The NXOpen.Routing.FittingOverstock object represents overstock applied over the faces of the routing parts. |
NXOpen.Routing.FittingOverstockBuilder |
Builder for creating or editing NXOpen.Routing.FittingOverstock objects. |
NXOpen.Routing.FittingOverstockCollection |
Represents a collection of NXOpen.Routing.FittingOverstock objects. |
NXOpen.Routing.FittingPort |
Represents a Routing Fitting Port Object:py:class:NXOpen.Routing.FittingPort. |
NXOpen.Routing.FittingPortCollection |
Represents a collection of NXOpen.Routing.FittingPort objects. |
NXOpen.Routing.FixturePort |
NXOpen.Routing.FixturePort objects are objects that |
NXOpen.Routing.FixturePortCollection |
Represents a collection of NXOpen.Routing.FixturePort objects. |
NXOpen.Routing.FormboardFrame |
The NXOpen.Routing.FormboardFrame is a (not pure) virtual class. |
NXOpen.Routing.FormboardFrameCGM |
Represents a Formboard Frame CGM. |
NXOpen.Routing.FormboardFrameCollection |
Represents a collection of NXOpen.Routing.FormboardFrame objects. |
NXOpen.Routing.FormboardFramePattern |
Represents a Formboard Frame Pattern. |
NXOpen.Routing.FormboardFrameRectangle |
Represents a Formboard Frame Rectangle. |
NXOpen.Routing.GapArcSegment |
Represents a gap arc segment. |
NXOpen.Routing.GapDisplayBuilder |
Builder for creating a gap arc object on a line segment. |
NXOpen.Routing.HandrailBuilder |
Represents a NXOpen.Routing.HandrailBuilder Creates a handrail from a selected point. |
NXOpen.Routing.HealPath |
Represents a NXOpen.Routing.HealPath object which holds the data used in the creation of the heal path spline. |
NXOpen.Routing.IAxisPort |
Interface class for all routing objects that specify a direction |
NXOpen.Routing.ICharacteristic |
Interface for querying and setting characteristic (UG attribute values) on various routing objects. |
NXOpen.Routing.IPath |
The Routing IPath object is a list of segments in a route. |
NXOpen.Routing.IRoutePosition |
Interface class for all routing objects that specify a single (possibly associative) location in space. |
NXOpen.Routing.ISegment |
Interface class for all routing segments [Line/Arc/Spline] |
NXOpen.Routing.ISegmentCollection |
Represents a collection of Routing.ISegment objects. |
NXOpen.Routing.InfoObjectsBuilder |
Represents a NXOpen.Routing.InfoObjectsBuilder |
NXOpen.Routing.InstanceNameLookupBuilder |
Represents a NXOpen.Routing.InstanceNameLookupBuilder . |
NXOpen.Routing.IntegrateRunsBuilder |
Builder Class for Integrate Runs Object |
NXOpen.Routing.InterfaceTerminalBase |
The NXOpen.Routing.InterfaceTerminalBase corresponds to an abstract class for a prototype NXOpen.Routing.Port . |
NXOpen.Routing.InterfaceTerminalRelationshipBase |
The abstract class NXOpen.Routing.InterfaceTerminalRelationshipBase relates many NXOpen.Routing.Port`s to one :py:class:`NXOpen.Routing.Port . |
NXOpen.Routing.InterfaceTerminalRelationshipCollection |
Represents a collection of NXOpen.Routing.InterfaceTerminalRelationshipShadow objects. |
NXOpen.Routing.InterfaceTerminalRelationshipShadow |
Represents an assembly shadow of NXOpen.Routing.InterfaceTerminalRelationshipBase . |
NXOpen.Routing.InterfaceTerminalShadow |
Represents the defining data for a physical NXOpen.Routing.Port . |
NXOpen.Routing.IsoDrawingBuilder |
Represents a NXOpen.Routing.IsoDrawingBuilder , used to run the ISOGEN engine to create isometric drawings of piping networks. |
NXOpen.Routing.ItemDefinition |
NXOpen.Routing.ItemDefinition object corresponds to DDID in AP212 and to a piece |
NXOpen.Routing.LineSegment |
Represents a line segment. |
NXOpen.Routing.LineSegmentCollection |
Represents a collection of NXOpen.Routing.LineSegment objects. |
NXOpen.Routing.LinearPathBuilder |
Builder for creating routing linear paths. |
NXOpen.Routing.LinearPathSettings |
Helper object used the by Routing.LinearPathBuilder builder. |
NXOpen.Routing.LogicalConnection |
Represents a connection between mutiple From and To Routing.LogicalTerminal . |
NXOpen.Routing.LogicalTerminal |
Assembly instance of a NXOpen.Routing.InterfaceTerminalBase . |
NXOpen.Routing.ManualRouteBuilder |
To create a new instance of this class, use NXOpen.Routing.RouteManager.CreateManualRouteBuilder |
NXOpen.Routing.MergeStocksBuilder |
Represents a NXOpen.Routing.MergeStocksBuilder Builder for merging routing stocks ( including space reservation stocks ). |
NXOpen.Routing.MiterCorner |
This class defines a mitered corner. |
NXOpen.Routing.MiterCornerCollection |
Represents a collection of NXOpen.Routing.MiterCorner objects. |
NXOpen.Routing.MiteredBendCorner |
Computes a fillet curve between two linear segments to form a smooth bend transition from one segment to another that represents a mitered bend. |
NXOpen.Routing.MiteredBendCornerCollection |
Represents a collection of NXOpen.Routing.MiteredBendCorner objects. |
NXOpen.Routing.ModelTerminalsBuilder |
The Builder to Model/UnModel the Terminals |
NXOpen.Routing.MultiPort |
Represents a NXOpen.Routing.MultiPort . |
NXOpen.Routing.MultiPortCollection |
Represents a collection of NXOpen.Routing.MultiPort objects. |
NXOpen.Routing.ObjectRelationship |
Represents a relationship between Routing objects. |
NXOpen.Routing.OffsetPath |
The Routing OffsetPath object is the set of information needed to define an offset route. |
NXOpen.Routing.OffsetPathCollection |
The Routing OffsetPath object is a list of segments in a route. |
NXOpen.Routing.Overstock |
Represents an NXOpen.Routing.Overstock object. |
NXOpen.Routing.OverstockApplication |
Represents a collection of NXOpen.Routing.OverstockApplication objects. |
NXOpen.Routing.OverstockApplicationCollection |
Represents a collection of NXOpen.Routing.OverstockApplication objects. |
NXOpen.Routing.OverstockBuilder |
Builder for creating/editing overstocks. |
NXOpen.Routing.OverstockFacesBuilder |
Builder for qualifying faces for overstock application over fittings. |
NXOpen.Routing.PartDefinitionBase |
The abstract class NXOpen.Routing.PartDefinitionBase contains information defining a logical part. |
NXOpen.Routing.PartDefinitionShadow |
NXOpen.Routing.PartDefinitionShadow contains the defining data for a |
NXOpen.Routing.Path |
The Routing Path object is the set of ordered continuous segments. |
NXOpen.Routing.PathStockBuilder |
Assigns stocks to segments based of users critiera and the current default stock. |
NXOpen.Routing.PlacePartBuilder |
To create a new instance of this class, use NXOpen.Routing.RouteManager.CreatePlacePartBuilderPTS |
NXOpen.Routing.PlacementSolutionsBuilder |
To create a new instance of this class, use NXOpen.Routing.RouteManager.CreatePlacementSolutionsBuilder |
NXOpen.Routing.Platform |
NXOpen.Routing.Platform objects are automatically created and updated by |
NXOpen.Routing.PlatformCreatorBuilder |
Builder for creating platform. |
NXOpen.Routing.PlatformFeature |
Represents a Platform feature. |
NXOpen.Routing.Port |
Routing Port Object is a parent class for FixturePort, ExtractPort, FittingPort, |
NXOpen.Routing.PortCollection |
Represents a collection of NXOpen.Routing.Port objects. |
NXOpen.Routing.PortConnection |
The Routing PortConnection object is used by Routing to position ports while placing parts. |
NXOpen.Routing.PortConnectionCollection |
Represents a collection of NXOpen.Routing.PortConnection objects. |
NXOpen.Routing.ProxyPort |
A NXOpen.Routing.ProxyPort is a port that represents a connector in another design zone, but not present in this design zone. |
NXOpen.Routing.ProxyPortCollection |
Represents a collection of NXOpen.Routing.ProxyPort objects. |
NXOpen.Routing.QuickPathBuilder |
Builder for creating a collision free path between points. |
NXOpen.Routing.RemoveDiscontinuityBuilder |
Builder class for remove discontinuity object |
NXOpen.Routing.ReuseLibrary |
Represents a NXOpen.Routing.ReuseLibrary |
NXOpen.Routing.RootObject |
The NXOpen.Routing.RootObject is the parent class of all other Routing logical objects. |
NXOpen.Routing.RouteLogicalAssociation |
RouteLogicalAssociation object associates non-electrical components to electrical components. |
NXOpen.Routing.RouteLogicalAssociationCollection |
Collection class for RouteLogicalAssociation object |
NXOpen.Routing.RouteManager |
Manages various Routing collections and methods for use in the current work part. |
NXOpen.Routing.RouteObject |
The Top level routing data model object. |
NXOpen.Routing.RouteObjectCollector |
Represents a NXOpen.Routing.RouteObjectCollector class to create objects for getting routing objects. |
NXOpen.Routing.RoutePartDescriptor |
Represents a part descriptor chrx. |
NXOpen.Routing.RoutePartDescriptorCollection |
Represents a collection of NXOpen.Routing.RoutePartDescriptor objects. |
NXOpen.Routing.RouteSegmentFont |
Represents a route segment font. |
NXOpen.Routing.RouteSegmentFontElement |
Represents a route segment font element. |
NXOpen.Routing.RouteSweptFoldBuilder |
Represents a Rout Swept Fold Builder |
NXOpen.Routing.RouteSweptTwistBuilder |
To create a new instance of this class, use NXOpen.Routing.RouteManager.CreateRouteSweptTwistBuilder |
NXOpen.Routing.RoutingMeasureDistanceBuilder |
Represents a NXOpen.Routing.RoutingMeasureDistanceBuilder |
NXOpen.Routing.RoutingSystem |
Routing object is a collection of NXOpen.Routing.Run objects. |
NXOpen.Routing.RoutingSystemCollection |
Represents a collection of NXOpen.Routing.RoutingSystem objects. |
NXOpen.Routing.Run |
Routing Run object references components and stocks which comprise a piping run. |
NXOpen.Routing.RunCollection |
Represents a collection of NXOpen.Routing.Run objects. |
NXOpen.Routing.RunItem |
Routing Run Item object references components which comprise a piping run. |
NXOpen.Routing.RunItemsBuilder |
The builder for creating the list item of RunItems |
NXOpen.Routing.RunItemsBuilderList |
Represents a list of objects. |
NXOpen.Routing.SBendCorner |
The Routing SBendCorner defines a S-Bend. |
NXOpen.Routing.SBendCornerCollection |
Represents a collection of NXOpen.Routing.SBendCorner objects. |
NXOpen.Routing.SegmentManager |
Contains the type of the routing part as well as the Collection objects for creating/iterating over routing objects. |
NXOpen.Routing.SegmentPairBuilder |
The builder for creating the list item of SegmentPairs |
NXOpen.Routing.SelectControlPoint |
Represents a single object selection. |
NXOpen.Routing.SelectISegment |
Represents a single object selection. |
NXOpen.Routing.SelectLineSegment |
Represents a single object selection. |
NXOpen.Routing.SelectPort |
Represents a single object selection. |
NXOpen.Routing.SelectRun |
Represents a single object selection. |
NXOpen.Routing.SelectStock |
Represents a single object selection. |
NXOpen.Routing.SimplifyPathBuilder |
Represents a NXOpen.Routing.SimplifyPathBuilder for Simplify Path operation. |
NXOpen.Routing.SingleDevice |
The Routing SingleDevice corresponds to an abstract instance of NXOpen.Routing.ItemDefinition . |
NXOpen.Routing.SpaceReservationBuilder |
Represents a NXOpen.Routing.SpaceReservationBuilder |
NXOpen.Routing.SplinePathBuilder |
Builder for creating a D-Cubed constrained spline. |
NXOpen.Routing.SplineSegment |
Represents a spline segment. |
NXOpen.Routing.SplineSegmentCollection |
Represents a collection of NXOpen.Routing.SplineSegment objects. |
NXOpen.Routing.SplitDuctBuilder |
Represents a NXOpen.Routing.SplitDuctBuilder |
NXOpen.Routing.SplitRunBuilder |
Builder Class for Split Run Object |
NXOpen.Routing.Stock |
The NXOpen.Routing.Stock object represents a material (such as as pipe or tube) that covers a path of segments. |
NXOpen.Routing.StockBrowserBuilder |
Builder class for stock browser . |
NXOpen.Routing.StockBuilder |
Builder for creating/editing stocks. |
NXOpen.Routing.StockCollection |
Represents a collection of NXOpen.Routing.Stock objects. |
NXOpen.Routing.StockColorBuilder |
Represents a NXOpen.Routing.StockColorBuilder . |
NXOpen.Routing.StockData |
A NXOpen.Routing.StockData contains the various profiles, characteristic information, NXOpen.Routing.Anchor and other attributes that define NXOpen.Routing.Stock objects. |
NXOpen.Routing.StockDataCollection |
Represents a collection of NXOpen.Routing.StockData objects. |
NXOpen.Routing.StockDefinition |
Represents Routing StockDefinition object |
NXOpen.Routing.StockDevice |
The Routing StockDevice corresponds to a generic stock instance of Routing.SingleDevice . |
NXOpen.Routing.StockOffsetPointBuilder |
Applies Assemblies Constraints to a selected NXOpen.Point or NXOpen.Routing.ControlPoint to mimic the update/move behavior of the input smart NXOpen.Point . |
NXOpen.Routing.StockOffsetPort |
NXOpen.Routing.StockOffsetPort class handles the relationship |
NXOpen.Routing.StockOffsetPortCollection |
Represents a collection of NXOpen.Routing.StockOffsetPort objects. |
NXOpen.Routing.StockPartConverterBuilder |
Represents a NXOpen.Routing.StockPartConverterBuilder Builder for Part Conversion of the stocks. |
NXOpen.Routing.StockPort |
NXOpen.Routing.StockPort objects are automatically created and updated by |
NXOpen.Routing.StockStyleBuilder |
Builder class to assigns style to the selected stock . |
NXOpen.Routing.StockTransition |
Represents NXOpen.Routing.StockTransition object. |
NXOpen.Routing.StockTransitionBuilder |
Builder for creating/editing stockTransition. |
NXOpen.Routing.SubdivideSegmentBuilder |
Represents a NXOpen.Routing.SubdivideSegmentBuilder . |
NXOpen.Routing.TerminalPort |
A NXOpen.Routing.TerminalPort models the pins on an electrical connector. |
NXOpen.Routing.TerminalPortBuilder |
Builder for creating the Terminal List Item for the ModelTerminals |
NXOpen.Routing.TerminalPortCollection |
The collection of all :py:class:`NXOpen.Routing.TerminalPort`s. |
NXOpen.Routing.TransformPathBuilder |
Builder for the “Transform Path” operation. |
NXOpen.Routing.UnifyPathBuilder |
Builder to unify Routing.Stock and Assemblies.Component based on specified characteristic values. |
NXOpen.Routing.WatertightFittingsBuilder |
Represents a NXOpen.Routing.WatertightFittingsBuilder |
NXOpen.Routing.WindCatcher |
Represents a Wind Catcher feature. |
NXOpen.Routing.WindCatcherBuilder |
Builder class for Wind Catcher feature. |
NXOpen.Routing.Wire |
The Routing Wire object is the set of information needed to define * a ROUTE_wire. |
NXOpen.Routing.WireCollection |
The Routing Wire object is a list of segments in a route and some stock. |