PortConnectionCollection Class¶
-
class
NXOpen.Routing.
PortConnectionCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.PortConnection
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CanPortsConnect | Determines if the two ports can be connected using a Port Connection object. |
CreatePortConnection | Creates a NXOpen.Routing.PortConnection object. |
Enumerations¶
PortConnectionCollectionPortsStatus Enumeration | Option to check if two ports can be connected by creating a NXOpen.Routing.PortConnection object. |
Method Detail¶
CanPortsConnect¶
-
PortConnectionCollection.
CanPortsConnect
¶ Determines if the two ports can be connected using a Port Connection object.
Signature
CanPortsConnect(port1, port2)
Parameters: - port1 (
NXOpen.Routing.Port
) – first Port to be connected by the Port Connection object - port2 (
NXOpen.Routing.Port
) – second Port to be connected by the Port Connection object
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
- port1 (
CreatePortConnection¶
-
PortConnectionCollection.
CreatePortConnection
¶ Creates a
NXOpen.Routing.PortConnection
object.Signature
CreatePortConnection(port1, port2)
Parameters: - port1 (
NXOpen.Routing.Port
) – first Port to be connected by the Port Connection object - port2 (
NXOpen.Routing.Port
) – second Port to be connected by the Port Connection object
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
- port1 (