Port Class¶
-
class
NXOpen.Routing.
Port
¶ Bases:
NXOpen.SmartObject
,NXOpen.Routing.IRoutePosition
Routing Port Object is a parent class for FixturePort, ExtractPort, FittingPort, Multiport, StockPort and TerminalPort
Creator not available in KF.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AllowMultipleConnections | Returns or sets the Allow Multiple Connections property for a NXOpen.Routing.Port . |
ClockIncrementObject | Returns or sets the clock angle increment expression of a NXOpen.Routing.Port , i. |
Color | Returns or sets the color of the object. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Point | Returns or sets the NXOpen.Point that specifies the location of the NXOpen.Routing.IRoutePosition object. |
Position | Returns or sets the current location of the object in ABS coordinates. |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Update | Returns the update option. |
Visibility | Returns the visibility. |
Methods¶
Method | Description |
---|---|
AskFeature | Ask NXOpen.Routing.FeaturePort object associated with NXOpen.Routing.Port . |
Blank | Blanks the object. |
Connect | Finds another NXOpen.Routing.Port to connect this port to. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteCharacterstics | Removes the input list of characteristics from this object. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
Disconnect | Deletes any NXOpen.Routing.PortConnection objects that reference this port. |
Evaluate | Evaluate a smart object. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FindPortIntegerCharacteristic | Searches for an integer characteristics on the port, then on the ports component and prototype port if the port is an occurrence. |
FindPortRealCharacteristic | Searches for a real characteristics on the port, then on the ports component and prototype port if the port is an occurrence. |
FindPortStringCharacteristic | Searches for a string characteristics on the port, then on the ports component and prototype port if the port is an occurrence. |
GetAlignmentVector | Retrieves the alignment vector of Port @return Vector direction in absolute co-ordinate system |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCharacteristics | Get all of the characteristics values on the this object. |
GetClockIncrement | The clock angle increment value of NXOpen.Routing.Port @return Clock increment value in degrees |
GetComponent | If this port is an occurrence, returns the component part to which it belongs. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetConnectedPorts | If port is connected to another port, returns both connected ports. |
GetControlPoint | Returns the Control Point to which this port is constrained, if any. |
GetCutbackLength | Returns the cutback length of a port, i. |
GetDestinationCharacteristics | Returns the destination characteristics from the input object. |
GetEngagement | Returns the engagement distance of a port, i. |
GetFlowDirection | Get the value of flow direction of NXOpen.Routing.Port @return |
GetForwardExtension | Returns the forward extension value for a port i. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerCharacteristic | Get the value of an integer characteristic associated with the input name. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetPortType | Get the type of Port @return Port Type |
GetRealAttribute | Gets a real attribute by title. |
GetRealCharacteristic | Get the value of a real characteristic associated with the input name. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetReferenceCharacteristic | Gets a reference characteristic from the port. |
GetRotationObject | Retrieves the object used to derive the rotation vector of Port @return Object used to derive the rotation vector |
GetRotationVector | Retrieves the rotation vector of Port @return Vector direction in absolute co-ordinate system |
GetSegment | Return the segment the port position and alignment are derived from Returns None if the port is not derived from segment @return ISegment from which the port is derived |
GetStringAttribute | Gets a string attribute value by title. |
GetStringCharacteristic | Get the value of a string characteristic associated with the input name. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Highlight | Highlights the object. |
IsEngagementLocked | Checks to see if ports are engaged. |
IsRotationLocked | Checks if ports have their rotation vectors locked. |
LockEngagement | Locks the port engagement using dcm3 constraints @return Newly created port constraints |
LockRotation | Locks the port rotation vector using dcm3 constraints @return Newly created port constraints |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveParameters | Removes the smart object parameters. |
RemoveViewDependency | Remove dependency on all views from an object. |
ReorderFeature | Reorders the NXOpen.Routing.FeaturePort object associated with NXOpen.Routing.Port after all of the features on which the port feature depends. |
ReplaceParameters | Edit a smart object by replacing its parameters using parameters of other smart object of the same class. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCharacteristic | Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. |
SetCharacteristics | Set all of the characteristics values on this object. |
SetClockIncrement | The clock angle increment value of NXOpen.Routing.Port |
SetFlowDirection | Set the flow direction value of NXOpen.Routing.Port |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetReferenceCharacteristic | Sets a reference characteristics on the port. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetVisibility | Sets the visibility. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
UnlockEngagement | Unlocks the port engagement |
UnlockRotation | Unlocks the port rotation |
Enumerations¶
PortCreateRotationVector Enumeration | Used by NXOpen.Routing.FittingPortCollection.CreateFromCsys and Routing.FixturePortCollection.CreateFromCsys to determine if the rotation vector on the port should be created. |
PortFlowDirectionType Enumeration | Allowed types for flow direction |
PortPortType Enumeration | Specifies the port type |
Property Detail¶
AllowMultipleConnections¶
-
Port.
AllowMultipleConnections
¶ Returns or sets the Allow Multiple Connections property for a
NXOpen.Routing.Port
.The property controls the number of connections that can be routed to this
NXOpen.Routing.Port
. Although this can be specified in the Mechanical application, the Electrical application is where this property is most used.-------------------------------------
Getter Method
Signature
AllowMultipleConnections()
Returns: Does this port allow multiple connections? Return type: bool New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AllowMultipleConnections(allowMultipleConnections)
Parameters: allowMultipleConnections (bool) – Should the multiport allow multiple connections? New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
ClockIncrementObject¶
-
Port.
ClockIncrementObject
¶ Returns or sets the clock angle increment expression of a
NXOpen.Routing.Port
, i.e. an expression representing the minimum angle for clocking the
NXOpen.Routing.Port
.-------------------------------------
Getter Method
Signature
ClockIncrementObject()
Returns: Clock increment expression Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ClockIncrementObject(increment)
Parameters: increment ( NXOpen.Expression
) – Clock increment expressionNew in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
IsOccurrence¶
-
Port.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Port.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Port.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Port.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Port.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Point¶
-
Port.
Point
¶ Returns or sets the
NXOpen.Point
that specifies the location of theNXOpen.Routing.IRoutePosition
object.A NULL object indicates that this object is not associated to any point.
-------------------------------------
Getter Method
Signature
Point()
Returns: New location of object in ABS coordinates Return type: NXOpen.Point
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) – New location of object in ABS coordinatesNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Position¶
-
Port.
Position
¶ Returns or sets the current location of the object in ABS coordinates.
This value is overridden by the coordinates of the point associated with this object.
-------------------------------------
Getter Method
Signature
Position()
Returns: Location of object in ABS coordinates Return type: NXOpen.Point3d
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Position(position)
Parameters: position ( NXOpen.Point3d
) – New location of object in ABS coordinatesNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Prototype¶
-
Port.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AskFeature¶
-
Port.
AskFeature
¶ Ask
NXOpen.Routing.FeaturePort
object associated withNXOpen.Routing.Port
.Returns None if the port was created in preNX6 release and not converted to
NXOpen.Routing.FeaturePort
. To convertNXOpen.Routing.Port
object toNXOpen.Routing.FeaturePort
object useRouting.PortCollection.ConvertToFeatures
.Signature
AskFeature()
Returns: Return type: NXOpen.Routing.FeaturePort
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
Connect¶
-
Port.
Connect
¶ Finds another
NXOpen.Routing.Port
to connect this port to.Builds a
NXOpen.Routing.PortConnection
object if a connectable port is found. SeeRouting.PortConnectionCollection.CanPortsConnect
. Does nothing if this port already has aNXOpen.Routing.PortConnection
object referencing it.Signature
Connect()
Returns: Return type: NXOpen.Routing.PortConnection
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
DeleteCharacterstics¶
-
Port.
DeleteCharacterstics
¶ Removes the input list of characteristics from this object.
Signature
DeleteCharacterstics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Disconnect¶
-
Port.
Disconnect
¶ Deletes any
NXOpen.Routing.PortConnection
objects that reference this port.Signature
Disconnect()
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
FindObject¶
-
Port.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
FindPortIntegerCharacteristic¶
-
Port.
FindPortIntegerCharacteristic
¶ Searches for an integer characteristics on the port, then on the ports component and prototype port if the port is an occurrence.
Signature
FindPortIntegerCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: int New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FindPortRealCharacteristic¶
-
Port.
FindPortRealCharacteristic
¶ Searches for a real characteristics on the port, then on the ports component and prototype port if the port is an occurrence.
Signature
FindPortRealCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FindPortStringCharacteristic¶
-
Port.
FindPortStringCharacteristic
¶ Searches for a string characteristics on the port, then on the ports component and prototype port if the port is an occurrence.
Signature
FindPortStringCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetAlignmentVector¶
-
Port.
GetAlignmentVector
¶ Retrieves the alignment vector of Port
Signature
GetAlignmentVector()
Returns: Vector direction in absolute co-ordinate system Return type: NXOpen.Vector3d
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetCharacteristics¶
-
Port.
GetCharacteristics
¶ Get all of the characteristics values on the this object.
Signature
GetCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetClockIncrement¶
-
Port.
GetClockIncrement
¶ The clock angle increment value of
NXOpen.Routing.Port
Signature
GetClockIncrement()
Returns: Clock increment value in degrees Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetComponent¶
-
Port.
GetComponent
¶ If this port is an occurrence, returns the component part to which it belongs.
Returns None otherwise.
Signature
GetComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX8.0.3.
License requirements: routing_base (“Routing Basic”)
GetConnectedPorts¶
-
Port.
GetConnectedPorts
¶ If port is connected to another port, returns both connected ports.
Returns None otherwise.
Signature
GetConnectedPorts()
Returns: a tuple Return type: A tuple consisting of (connectedPort1, connectedPort2). connectedPort1 is a NXOpen.Routing.Port
. connectedPort2 is aNXOpen.Routing.Port
.New in version NX10.0.0.
License requirements: routing_base (“Routing Basic”)
GetControlPoint¶
-
Port.
GetControlPoint
¶ Returns the Control Point to which this port is constrained, if any.
Returns None otherwise.
Signature
GetControlPoint()
Returns: Return type: NXOpen.Routing.ControlPoint
New in version NX8.0.3.
License requirements: routing_base (“Routing Basic”)
GetCutbackLength¶
-
Port.
GetCutbackLength
¶ Returns the cutback length of a port, i.
e. the length along the wire from * the port where individual wires leave a bundle to attach to pins
Signature
GetCutbackLength()
Returns: Cutback length Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetDestinationCharacteristics¶
-
Port.
GetDestinationCharacteristics
¶ Returns the destination characteristics from the input object.
Retrieves the description of which destination characteristics to read from the application view and then reads those destination characteristics from the object
- Ports: Reads characteristics from the port.
- RCPs: Attempts to find a port at the RCP, reads characteristics from
the port if it exists, otherwise reads from the stock associated with the rcp.
- Segments: Reads characteristics from the stock associated with the segment.
- Components: Reads characteristics directly from the component.
- Stock: Reads characteristics from the stock or from the stock’s data.
Signature
GetDestinationCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetEngagement¶
-
Port.
GetEngagement
¶ Returns the engagement distance of a port, i.
e. the distance * behind the port that another fitting or stock may engage
Signature
GetEngagement()
Returns: Engagement distance Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetFlowDirection¶
-
Port.
GetFlowDirection
¶ Get the value of flow direction of
NXOpen.Routing.Port
Signature
GetFlowDirection()
Returns: Return type: NXOpen.Routing.PortFlowDirectionType
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
GetForwardExtension¶
-
Port.
GetForwardExtension
¶ Returns the forward extension value for a port i.
e. the minimum length that * a segment must remain straight coming out of a
NXOpen.Routing.Port
Signature
GetForwardExtension()
Returns: Port extension Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetIntegerCharacteristic¶
-
Port.
GetIntegerCharacteristic
¶ Get the value of an integer characteristic associated with the input name.
Signature
GetIntegerCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: int New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetPortType¶
-
Port.
GetPortType
¶ Get the type of Port
Signature
GetPortType()
Returns: Port Type Return type: NXOpen.Routing.PortPortType
New in version NX7.5.2.
License requirements: routing_base (“Routing Basic”)
GetRealCharacteristic¶
-
Port.
GetRealCharacteristic
¶ Get the value of a real characteristic associated with the input name.
Signature
GetRealCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetReferenceCharacteristic¶
-
Port.
GetReferenceCharacteristic
¶ Gets a reference characteristic from the port.
Signature
GetReferenceCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: str New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
GetRotationObject¶
-
Port.
GetRotationObject
¶ Retrieves the object used to derive the rotation vector of Port
Signature
GetRotationObject()
Returns: Object used to derive the rotation vector Return type: NXOpen.DisplayableObject
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetRotationVector¶
-
Port.
GetRotationVector
¶ Retrieves the rotation vector of Port
Signature
GetRotationVector()
Returns: Vector direction in absolute co-ordinate system Return type: NXOpen.Vector3d
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetSegment¶
-
Port.
GetSegment
¶ Return the segment the port position and alignment are derived from Returns None if the port is not derived from segment
Signature
GetSegment()
Returns: ISegment from which the port is derived Return type: NXOpen.Routing.ISegment
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetStringCharacteristic¶
-
Port.
GetStringCharacteristic
¶ Get the value of a string characteristic associated with the input name.
Signature
GetStringCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
IsEngagementLocked¶
-
Port.
IsEngagementLocked
¶ Checks to see if ports are engaged.
Signature
IsEngagementLocked(portToCheck)
Parameters: portToCheck ( NXOpen.Routing.Port
) –Returns: Return type: bool New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
IsRotationLocked¶
-
Port.
IsRotationLocked
¶ Checks if ports have their rotation vectors locked.
Signature
IsRotationLocked(portToCheck)
Parameters: portToCheck ( NXOpen.Routing.Port
) –Returns: Return type: bool New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
LockEngagement¶
-
Port.
LockEngagement
¶ Locks the port engagement using dcm3 constraints
Signature
LockEngagement(portToLock)
Parameters: portToLock ( NXOpen.Routing.Port
) –Returns: Newly created port constraints Return type: list of NXOpen.Positioning.Constraint
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
LockRotation¶
-
Port.
LockRotation
¶ Locks the port rotation vector using dcm3 constraints
Signature
LockRotation(portToLock)
Parameters: portToLock ( NXOpen.Routing.Port
) –Returns: Newly created port constraints Return type: list of NXOpen.Positioning.Constraint
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
Print¶
-
Port.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
ReorderFeature¶
-
Port.
ReorderFeature
¶ Reorders the
NXOpen.Routing.FeaturePort
object associated withNXOpen.Routing.Port
after all of the features on which the port feature depends.Does nothing if the port was created in preNX6 release and not converted to
NXOpen.Routing.FeaturePort
. To convertNXOpen.Routing.Port
object toNXOpen.Routing.FeaturePort
object useRouting.PortCollection.ConvertToFeatures
.Signature
ReorderFeature()
New in version NX6.0.5.
License requirements: routing_base (“Routing Basic”)
SetCharacteristic¶
-
Port.
SetCharacteristic
¶ Overloaded method SetCharacteristic
SetCharacteristic(name, value)
SetCharacteristic(name, value)
SetCharacteristic(name, value)
-------------------------------------
Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to integer if it’s type is not integer.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (int) –
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an real characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to real if it’s type is not real.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (float) –
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an string characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to string if it’s type is not string.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristics¶
-
Port.
SetCharacteristics
¶ Set all of the characteristics values on this object.
Signature
SetCharacteristics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetClockIncrement¶
-
Port.
SetClockIncrement
¶ The clock angle increment value of
NXOpen.Routing.Port
Signature
SetClockIncrement(increment)
Parameters: increment (float) – Clock increment value in degrees New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetFlowDirection¶
-
Port.
SetFlowDirection
¶ Set the flow direction value of
NXOpen.Routing.Port
Signature
SetFlowDirection(flowDirection)
Parameters: flowDirection ( NXOpen.Routing.PortFlowDirectionType
) –New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
SetName¶
-
Port.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetReferenceCharacteristic¶
-
Port.
SetReferenceCharacteristic
¶ Sets a reference characteristics on the port.
Signature
SetReferenceCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
UnlockEngagement¶
-
Port.
UnlockEngagement
¶ Unlocks the port engagement
Signature
UnlockEngagement(portToUnlock)
Parameters: portToUnlock ( NXOpen.Routing.Port
) –New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
UnlockRotation¶
-
Port.
UnlockRotation
¶ Unlocks the port rotation
Signature
UnlockRotation(portToUnlock)
Parameters: portToUnlock ( NXOpen.Routing.Port
) –New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)