PortCreateRotationVector Enumeration¶
NXOpen.Routing.Port.CreateRotationVector is an alias for NXOpen.Routing.PortCreateRotationVector
-
class
NXOpen.Routing.
PortCreateRotationVector
¶ Bases:
object
Used by
NXOpen.Routing.FittingPortCollection.CreateFromCsys
andRouting.FixturePortCollection.CreateFromCsys
to determine if the rotation vector on the port should be created.Enum Members
Enum Member Enum Member Description No Do not create the rotation vector on the port created from a coordinate system.Yes Create the rotation vector on the port created from a coordinate system.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-