FittingPortCollection Class¶
-
class
NXOpen.Routing.
FittingPortCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.FittingPort
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateFittingPort | Creates a FittingPort with a rotation vector at an absolute location. |
CreateFromAxis | Creates a fitting port based on an existing axis. |
CreateFromCsys | Creates a fitting port based on an existing Cartesian Coordinate System. |
Method Detail¶
CreateFittingPort¶
-
FittingPortCollection.
CreateFittingPort
¶ Overloaded method CreateFittingPort
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle)
CreateFittingPort(origin, alignmentVector)
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, point)
CreateFittingPort(origin, alignmentVector, point)
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, axis)
CreateFittingPort(origin, alignmentVector, derivationObject)
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, allowMultipleConnections)
CreateFittingPort(origin, alignmentVector, allowMultipleConnections)
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, point, allowMultipleConnections)
CreateFittingPort(origin, alignmentVector, point, allowMultipleConnections)
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, axis, allowMultipleConnections)
CreateFittingPort(origin, alignmentVector, derivationObject, allowMultipleConnections)
-------------------------------------
Creates a FittingPort with a rotation vector at an absolute location. Default allows multiple connections to this port.
Signature
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fitting port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FittingPort with no rotation vector at an absolute location. Default allows multiple connections to this port.
Signature
CreateFittingPort(origin, alignmentVector)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FittingPort with a rotation vector at a point. Default allows multiple connections to this port.
Signature
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, point)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fitting port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
- point (
NXOpen.Point
) – Fitting Port derived from this point
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FittingPort with no rotation vector at a point. Default allows multiple connections to this port.
Signature
CreateFittingPort(origin, alignmentVector, point)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port - point (
NXOpen.Point
) – Fitting Port derived from this point
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FittingPort with a rotation vector on an axis. Default allows multiple connections to this port.
Signature
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, axis)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fitting port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
- axis (
NXOpen.Axis
) – Fitting Port derived from this axis
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FittingPort with no rotation vector on an axis. Default allows multiple connections to this port.
Signature
CreateFittingPort(origin, alignmentVector, derivationObject)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port - derivationObject (
NXOpen.Axis
) – Fitting Port derived from this axis
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FittingPort with a rotation vector at an absolute location
Signature
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fitting port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
- allowMultipleConnections (bool) – Does this fitting port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FittingPort with no rotation vector at an absolute location
Signature
CreateFittingPort(origin, alignmentVector, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port - allowMultipleConnections (bool) – Does this fitting port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FittingPort with a rotation vector at a point
Signature
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, point, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fitting port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
- point (
NXOpen.Point
) – Fitting Port derived from this point - allowMultipleConnections (bool) – Does this fitting port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FittingPort with no rotation vector at a point
Signature
CreateFittingPort(origin, alignmentVector, point, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port - point (
NXOpen.Point
) – Fitting Port derived from this point - allowMultipleConnections (bool) – Does this fitting port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FittingPort with a rotation vector on an axis
Signature
CreateFittingPort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, axis, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fitting port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
- axis (
NXOpen.Axis
) – Fitting Port derived from this axis - allowMultipleConnections (bool) – Does this fitting port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FittingPort with no rotation vector on an axis
Signature
CreateFittingPort(origin, alignmentVector, derivationObject, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fitting port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fitting port - derivationObject (
NXOpen.Axis
) – Fitting Port derived from this axis - allowMultipleConnections (bool) – Does this fitting port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
CreateFromAxis¶
-
FittingPortCollection.
CreateFromAxis
¶ Creates a fitting port based on an existing axis.
Signature
CreateFromAxis(axis)
Parameters: axis ( NXOpen.Axis
) – The new Fitting Port will be derived from this axisReturns: Return type: NXOpen.Routing.FittingPort
New in version NX10.0.0.
License requirements: routing_base (“Routing Basic”)
CreateFromCsys¶
-
FittingPortCollection.
CreateFromCsys
¶ Creates a fitting port based on an existing Cartesian Coordinate System.
The port aligns with the Z axis of the Coordinate System. The port’s rotation vector, if any, aligns with the Y direction of the Coordinate System.
Signature
CreateFromCsys(csys, createRotationVector)
Parameters: - csys (
NXOpen.CartesianCoordinateSystem
) – The new Fitting Port will be derived from this Cartesian Coordinate System - createRotationVector (
NXOpen.Routing.PortCreateRotationVector
) – Should the rotation vector be created?
Returns: Return type: New in version NX10.0.0.
License requirements: routing_base (“Routing Basic”)
- csys (