WatertightFittingsBuilder Class¶
-
class
NXOpen.Routing.
WatertightFittingsBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Routing.WatertightFittingsBuilder
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateWatertightFittingsBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Filename | Returns or sets the name of new part file containing watertight fittings assembly which includes the full path. |
FittingMembers | Returns the Routing Object Collector builder that stores selected routing members |
FlangeDirection | Returns or sets the direction of flange thickness |
FlangeOffset | Returns the offset value for flange creation |
FlangeSketch | Returns the section used for creating penetration extrude. |
FlangeThickness | Returns the thickness value for flange creation |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOptionalAttributes | Get optional attributes for Watertight Fittings. |
GetRequiredAttributes | Get required attributes for Watertight Fittings. |
SetOptionalAttributes | Set optional attributes for Watertight Fittings. |
SetRequiredAttributes | Set required attributes for Watertight Fittings. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Filename¶
-
WatertightFittingsBuilder.
Filename
¶ Returns or sets the name of new part file containing watertight fittings assembly which includes the full path.
-------------------------------------
Getter Method
Signature
Filename()
Returns: Return type: str New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Filename(fileName)
Parameters: fileName (str) – New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FittingMembers¶
-
WatertightFittingsBuilder.
FittingMembers
¶ Returns the Routing Object Collector builder that stores selected routing members
-------------------------------------
Getter Method
Signature
FittingMembers()
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FlangeDirection¶
-
WatertightFittingsBuilder.
FlangeDirection
¶ Returns or sets the direction of flange thickness
-------------------------------------
Getter Method
Signature
FlangeDirection()
Returns: Return type: bool New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
FlangeDirection(flangeDirection)
Parameters: flangeDirection (bool) – New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FlangeOffset¶
-
WatertightFittingsBuilder.
FlangeOffset
¶ Returns the offset value for flange creation
-------------------------------------
Getter Method
Signature
FlangeOffset()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FlangeSketch¶
-
WatertightFittingsBuilder.
FlangeSketch
¶ Returns the section used for creating penetration extrude.
-------------------------------------
Getter Method
Signature
FlangeSketch()
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FlangeThickness¶
-
WatertightFittingsBuilder.
FlangeThickness
¶ Returns the thickness value for flange creation
-------------------------------------
Getter Method
Signature
FlangeThickness()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
GetOptionalAttributes¶
-
WatertightFittingsBuilder.
GetOptionalAttributes
¶ Get optional attributes for Watertight Fittings.
Signature
GetOptionalAttributes()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetRequiredAttributes¶
-
WatertightFittingsBuilder.
GetRequiredAttributes
¶ Get required attributes for Watertight Fittings.
Signature
GetRequiredAttributes()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetOptionalAttributes¶
-
WatertightFittingsBuilder.
SetOptionalAttributes
¶ Set optional attributes for Watertight Fittings.
Signature
SetOptionalAttributes(charxData)
Parameters: charxData ( NXOpen.Routing.CharacteristicList
) –New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetRequiredAttributes¶
-
WatertightFittingsBuilder.
SetRequiredAttributes
¶ Set required attributes for Watertight Fittings.
Signature
SetRequiredAttributes(charxData)
Parameters: charxData ( NXOpen.Routing.CharacteristicList
) –New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Validate¶
-
WatertightFittingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.