RouteLogicalAssociationCollection Class¶
-
class
NXOpen.Routing.
RouteLogicalAssociationCollection
¶ Bases:
object
Collection class for RouteLogicalAssociation object
To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateLogicalAssociation | Creates a NXOpen.Routing.RouteLogicalAssociation @return Logical Association |
GetLogicalAssociations | Returns NXOpen.Routing.RouteLogicalAssociation of this part. |
PerformLogicalAssociation | Performs the blanking/suppressing of objects in NXOpen.Routing.RouteLogicalAssociation . |
Method Detail¶
CreateLogicalAssociation¶
-
RouteLogicalAssociationCollection.
CreateLogicalAssociation
¶ Creates a
NXOpen.Routing.RouteLogicalAssociation
Signature
CreateLogicalAssociation(name, control, targets, includeStocks)
Parameters: - name (str) – Name of Logical Association NOTE: The full Unicode character set is not supported for this parameter.
- control (
NXOpen.NXObject
) – Control object - targets (list of
NXOpen.NXObject
) – Targets for Logical Association - includeStocks (bool) – Include all stocks in the logical association
Returns: Logical Association
Return type: New in version NX4.0.0.
License requirements: routing_harness (“Routing Harness”)
GetLogicalAssociations¶
-
RouteLogicalAssociationCollection.
GetLogicalAssociations
¶ Returns
NXOpen.Routing.RouteLogicalAssociation
of this part.Signature
GetLogicalAssociations()
Returns: Return type: list of NXOpen.Routing.RouteLogicalAssociation
New in version NX5.0.0.
License requirements: routing_harness (“Routing Harness”)
PerformLogicalAssociation¶
-
RouteLogicalAssociationCollection.
PerformLogicalAssociation
¶ Performs the blanking/suppressing of objects in
NXOpen.Routing.RouteLogicalAssociation
.Signature
PerformLogicalAssociation(logicalAssociations)
Parameters: logicalAssociations (list of NXOpen.Routing.RouteLogicalAssociation
) –New in version NX5.0.0.
License requirements: routing_harness (“Routing Harness”)