DuctSizeCalculatorBuilder Class¶
-
class
NXOpen.Routing.
DuctSizeCalculatorBuilder
¶ Bases:
NXOpen.Builder
Builder to perform calculations of the duct which is to be used in the HVAC applications.
The duct has some flow attributes and has dimentions. To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateDuctSizeCalculatorBuilder
Default values.
Property Value DuctAreaExp.Value 0 (millimeters part), 0 (inches part) DuctAspectRatioExp.Value 0 DuctDiameterExp.Value 0 (millimeters part), 0 (inches part) DuctEqvalentDiameterExp.Value 0 (millimeters part), 0 (inches part) DuctHeightExp.Value 0 (millimeters part), 0 (inches part) DuctShape Rectangular DuctWidthExp.Value 0 (millimeters part), 0 (inches part) IsCreateSpaceReservationEnabled 0 IsDisplayFlowParamsEnabled 0 VelocityExp.Value 0 (millimeters part), 0 (inches part) VolumeFlowRateExp.Value 0 (millimeters part), 0 (inches part) New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
DuctAreaExp | Returns the duct area |
DuctAspectRatioExp | Returns the Aspect ratio of the duct dimentions |
DuctDiameterExp | Returns the duct diameter |
DuctEqvalentDiameterExp | Returns the duct equivalent diameter |
DuctHeightExp | Returns the duct height |
DuctShape | Returns or sets the shape of the duct |
DuctWidthExp | Returns the duct width |
IsCreateSpaceReservationEnabled | Returns or sets the status of the create space reservation toggle; whether the toggle is on or off. |
IsDisplayFlowParamsEnabled | Returns or sets the ON or OFF status of the Display flow parameters over Segments toggle |
RouteObjectCollector | Returns the route object collector Stores the routing segments for which calculations are to be done |
Tag | Returns the Tag for this object. |
VelocityExp | Returns the velocity component Flow parameter for the duct. |
VolumeFlowRateExp | Returns the volume flow rate associated with the duct. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DuctSizeCalculatorBuilderDuctShapeType Enumeration | This enum represents the shape of the duct |
Property Detail¶
DuctAreaExp¶
-
DuctSizeCalculatorBuilder.
DuctAreaExp
¶ Returns the duct area
-------------------------------------
Getter Method
Signature
DuctAreaExp()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
DuctAspectRatioExp¶
-
DuctSizeCalculatorBuilder.
DuctAspectRatioExp
¶ Returns the Aspect ratio of the duct dimentions
-------------------------------------
Getter Method
Signature
DuctAspectRatioExp()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
DuctDiameterExp¶
-
DuctSizeCalculatorBuilder.
DuctDiameterExp
¶ Returns the duct diameter
-------------------------------------
Getter Method
Signature
DuctDiameterExp()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
DuctEqvalentDiameterExp¶
-
DuctSizeCalculatorBuilder.
DuctEqvalentDiameterExp
¶ Returns the duct equivalent diameter
-------------------------------------
Getter Method
Signature
DuctEqvalentDiameterExp()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
DuctHeightExp¶
-
DuctSizeCalculatorBuilder.
DuctHeightExp
¶ Returns the duct height
-------------------------------------
Getter Method
Signature
DuctHeightExp()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
DuctShape¶
-
DuctSizeCalculatorBuilder.
DuctShape
¶ Returns or sets the shape of the duct
-------------------------------------
Getter Method
Signature
DuctShape()
Returns: Return type: NXOpen.Routing.DuctSizeCalculatorBuilderDuctShapeType
New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
-------------------------------------
Setter Method
Signature
DuctShape(ductShape)
Parameters: ductShape ( NXOpen.Routing.DuctSizeCalculatorBuilderDuctShapeType
) –New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
DuctWidthExp¶
-
DuctSizeCalculatorBuilder.
DuctWidthExp
¶ Returns the duct width
-------------------------------------
Getter Method
Signature
DuctWidthExp()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
IsCreateSpaceReservationEnabled¶
-
DuctSizeCalculatorBuilder.
IsCreateSpaceReservationEnabled
¶ Returns or sets the status of the create space reservation toggle; whether the toggle is on or off.
-------------------------------------
Getter Method
Signature
IsCreateSpaceReservationEnabled()
Returns: Return type: bool New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
-------------------------------------
Setter Method
Signature
IsCreateSpaceReservationEnabled(isCreateSpaceReservation)
Parameters: isCreateSpaceReservation (bool) – New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
IsDisplayFlowParamsEnabled¶
-
DuctSizeCalculatorBuilder.
IsDisplayFlowParamsEnabled
¶ Returns or sets the ON or OFF status of the Display flow parameters over Segments toggle
-------------------------------------
Getter Method
Signature
IsDisplayFlowParamsEnabled()
Returns: Return type: bool New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
-------------------------------------
Setter Method
Signature
IsDisplayFlowParamsEnabled(isDispFlowParams)
Parameters: isDispFlowParams (bool) – New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
RouteObjectCollector¶
-
DuctSizeCalculatorBuilder.
RouteObjectCollector
¶ Returns the route object collector Stores the routing segments for which calculations are to be done
-------------------------------------
Getter Method
Signature
RouteObjectCollector()
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
VelocityExp¶
-
DuctSizeCalculatorBuilder.
VelocityExp
¶ Returns the velocity component Flow parameter for the duct.
-------------------------------------
Getter Method
Signature
VelocityExp()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
VolumeFlowRateExp¶
-
DuctSizeCalculatorBuilder.
VolumeFlowRateExp
¶ Returns the volume flow rate associated with the duct.
This is a flow parameter
-------------------------------------
Getter Method
Signature
VolumeFlowRateExp()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: routing_hvac (“Routing HVAC”)
Method Detail¶
Validate¶
-
DuctSizeCalculatorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.