BendCorner Class¶
-
class
NXOpen.Routing.
BendCorner
¶ Bases:
NXOpen.Routing.Corner
Computes a fillet curve between two linear segments to form a smooth bend transition from one segment to another.
To create a new instance of this class, use
NXOpen.Routing.BendCornerCollection.CreateCorner
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BendMethod | Returns or sets the bend method |
BendRadius | Returns or sets the bend radius of the corner. |
BendRatio | Returns or sets the bend ratio to apply when computing the bend radius |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Rcp | Returns or sets the corner ControlPoint referenced by the Corner object. |
Tag | Returns the Tag for this object. |
UseBendRatio | Returns or sets whether or not to compute the bend radius as a ratio of the stock diameter. |
Methods¶
Method | Description |
---|---|
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FindSideSegments | Returns the straight line segments attached to the fillet curve of this bend corner. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSegment | The bend segment following the fillet curve created for the bend. |
GetStocks | Returns the stocks that are assigned to segments affected by * this corner object. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
BendMethod¶
-
BendCorner.
BendMethod
¶ Returns or sets the bend method
-------------------------------------
Getter Method
Signature
BendMethod()
Returns: Return type: NXOpen.Routing.CornerTypeBuilderBendMethods
New in version NX8.5.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
BendMethod(bendMethod)
Parameters: bendMethod ( NXOpen.Routing.CornerTypeBuilderBendMethods
) –New in version NX8.5.0.
License requirements: routing_base (“Routing Basic”)
BendRadius¶
-
BendCorner.
BendRadius
¶ Returns or sets the bend radius of the corner.
-------------------------------------
Getter Method
Signature
BendRadius()
Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
BendRadius(bendRadius)
Parameters: bendRadius (float) – the the bend radius. New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
BendRatio¶
-
BendCorner.
BendRatio
¶ Returns or sets the bend ratio to apply when computing the bend radius
-------------------------------------
Getter Method
Signature
BendRatio()
Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
BendRatio(bendRatio)
Parameters: bendRatio (float) – the bend ratio. New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
IsOccurrence¶
-
BendCorner.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
BendCorner.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
BendCorner.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
BendCorner.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
BendCorner.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
BendCorner.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
UseBendRatio¶
-
BendCorner.
UseBendRatio
¶ Returns or sets whether or not to compute the bend radius as a ratio of the stock diameter.
-------------------------------------
Getter Method
Signature
UseBendRatio()
Returns: Return type: bool New in version NX4.0.0.
Deprecated since version NX8.5.0: Use
Routing.BendCorner.BendMethod
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
UseBendRatio(useBendRatio)
Parameters: useBendRatio (bool) – the use bend ratio. New in version NX4.0.0.
Deprecated since version NX8.5.0: Use
Routing.BendCorner.BendMethod
instead.License requirements: routing_base (“Routing Basic”)
Method Detail¶
FindObject¶
-
BendCorner.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
FindSideSegments¶
-
BendCorner.
FindSideSegments
¶ Returns the straight line segments attached to the fillet curve of this bend corner.
Signature
FindSideSegments()
Returns: the side segments. There will be from 0 to 2 total side segments. :rtype: list of
NXOpen.Curve
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
GetSegment¶
-
BendCorner.
GetSegment
¶ The bend segment following the fillet curve created for the bend.
Signature
GetSegment()
Returns: Return type: NXOpen.Routing.ISegment
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Print¶
-
BendCorner.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
BendCorner.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.