BendCornerCollection Class¶
-
class
NXOpen.Routing.
BendCornerCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.BendCorner
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
AssignCornerByBendRadius | This routine assigns a new bend corner to the given input bend corner object using bend radius. |
AssignCornerByBendRatio | This routine assigns a new bend corner to the given input bend corner object using bend ratio. |
AssignCornerByBendTable | This routine assigns a bend corner to the given input RCP object using a bend table entry. |
Create | Create a bend corner object at a Control Point. |
CreateCorner | Create a bend corner object at a Control Point. |
GetBendAssociatedToSegment | Enquire the Bend Corner that this segment represents. |
Enumerations¶
BendCornerCollectionType Enumeration | Option for creating a bend using a bend table or using radius or ratio |
Method Detail¶
AssignCornerByBendRadius¶
-
BendCornerCollection.
AssignCornerByBendRadius
¶ This routine assigns a new bend corner to the given input bend corner object using bend radius.
This “assignment” can involve the removal of an existing corner at this location and the creation of a new corner.
Signature
AssignCornerByBendRadius(bendCrn, bendRadius)
Parameters: - bendCrn (
NXOpen.Routing.ControlPoint
) – Input bend corner. - bendRadius (float) – Radius of bend corner arc.
Returns: The newly created Bend Corner
Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
- bendCrn (
AssignCornerByBendRatio¶
-
BendCornerCollection.
AssignCornerByBendRatio
¶ This routine assigns a new bend corner to the given input bend corner object using bend ratio.
This “assignment” can involve the removal of an existing corner at this location and the creation of a new corner.
Signature
AssignCornerByBendRatio(bendCrn, bendRatio)
Parameters: - bendCrn (
NXOpen.Routing.ControlPoint
) – Input bend corner. - bendRatio (float) – Bend ratio must be greater than 0.5.
Returns: The newly created Bend Corner
Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
- bendCrn (
AssignCornerByBendTable¶
-
BendCornerCollection.
AssignCornerByBendTable
¶ This routine assigns a bend corner to the given input RCP object using a bend table entry.
This “assignment” can involve the removal of an existing corner at this location and the creation of a new corner. The application view must be loaded before attempting to assign a bend corner of this type.
Signature
AssignCornerByBendTable(rcp, bendTable)
Parameters: - rcp (
NXOpen.Routing.ControlPoint
) – Control point to assign corner to. None not allowed. - bendTable (str) – The bend table entry that is used to create bend corner NOTE: The full Unicode character set is not supported for this parameter.
Returns: The newly created Bend Corner
Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
- rcp (
Create¶
-
BendCornerCollection.
Create
¶ Create a bend corner object at a Control Point.
Signature
Create(rcp, useBendRatio, bendRatio, bendRadius)
Parameters: - rcp (
NXOpen.Routing.ControlPoint
) – Route control point to bend. - useBendRatio (bool) – TRUE: use bend ratio calculation, FALSE: use given radius
- bendRatio (float) – Bend ratio only used if use_bend_ratio is TRUE. Must be greater than 0.5.
- bendRadius (float) – Radius of bend corner arc, only used if use_bend_ratio is FALSE. Must be greater than 0.
Returns: The new bend corner.
Return type: New in version NX4.0.0.
Deprecated since version NX8.5.0: Use
Routing.BendCornerCollection.CreateCorner
instead.License requirements: routing_base (“Routing Basic”)
- rcp (
CreateCorner¶
-
BendCornerCollection.
CreateCorner
¶ Create a bend corner object at a Control Point.
Signature
CreateCorner(rcp, bendMethod, bendRatio, bendRadius)
Parameters: - rcp (
NXOpen.Routing.ControlPoint
) – Route control point to bend. - bendMethod (
NXOpen.Routing.CornerTypeBuilderBendMethods
) – Enumerated bend method. - bendRatio (float) – Bend ratio is used only if bend method is set to
NXOpen.Routing.CornerTypeBuilderBendMethods.RatioToDiameter
. Must be greater than 0.5. - bendRadius (float) – Radius of bend corner arc, used only if bend method is set to
NXOpen.Routing.CornerTypeBuilderBendMethods.Radius
. Must be greater than 0.
Returns: The new bend corner.
Return type: New in version NX8.5.0.
License requirements: routing_base (“Routing Basic”)
- rcp (
GetBendAssociatedToSegment¶
-
BendCornerCollection.
GetBendAssociatedToSegment
¶ Enquire the Bend Corner that this segment represents.
(None can be returned, indicating that this segment does not represent a Bend Corner.)
Signature
GetBendAssociatedToSegment(segment)
Parameters: segment ( NXOpen.Routing.ISegment
) – Segment being queried for the Bend Corner it represents.Returns: Bend Corner that segment represents (None can be returned,indicating that segment does not represent a Bend Corner). :rtype:
NXOpen.Routing.BendCorner
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)