DuctReinforcementBuilder Class¶
-
class
NXOpen.Routing.
DuctReinforcementBuilder
¶ Bases:
NXOpen.Builder
Builder for creating/editing duct reinforcements.
Rules can be defined based on which the type of reinforcement to be placed on the input duct will be determined. See
NXOpen.Routing.DuctReinforcement
for Duct Reinforcement class documentation.To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateDuctReinforcementBuilder
Default values.
Property Value IntervalExpression.Value 100 (millimeters part), 4 (inches part) NumberOfPairs 1 ReinforcementType None SpacingExpression.Value 50 (millimeters part), 2 (inches part) New in version NX8.5.2.
Properties¶
Property | Description |
---|---|
IntervalExpression | Returns the distance between each set of reinforcement stocks going perpendicular to axis of the duct |
MinimumClearance | Returns the minimum clearance value for duct reinforcement It defines the minimum distance from the beginning and end of the path to place the first and last piece of reinforcement stock. |
NumberOfPairs | Returns or sets the number of pairs of outside reinforcements going parallel to axis of the duct |
ParallelReinforcement | Returns or sets the stock settings for parallel reinforcements |
ParentDuct | Returns the duct that is to be reinforced. |
PathCurve | Returns the path curve that is used to specify perpendicular reinforcement defining points. |
PerpendicularReinforcement | Returns or sets the stock settings for perpendicular reinforcements |
ReinforcementType | Returns or sets the type of reinforcement |
SpacingExpression | Returns the distance between each pair of reinforcement |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdatePathCurve | The path curve that is used to specify perpendicular reinforcement defining points. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DuctReinforcementBuilderReinforcementTypes Enumeration | Specifies the type of duct reinforcements. |
Property Detail¶
IntervalExpression¶
-
DuctReinforcementBuilder.
IntervalExpression
¶ Returns the distance between each set of reinforcement stocks going perpendicular to axis of the duct
-------------------------------------
Getter Method
Signature
IntervalExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
MinimumClearance¶
-
DuctReinforcementBuilder.
MinimumClearance
¶ Returns the minimum clearance value for duct reinforcement It defines the minimum distance from the beginning and end of the path to place the first and last piece of reinforcement stock.
-------------------------------------
Getter Method
Signature
MinimumClearance()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
NumberOfPairs¶
-
DuctReinforcementBuilder.
NumberOfPairs
¶ Returns or sets the number of pairs of outside reinforcements going parallel to axis of the duct
-------------------------------------
Getter Method
Signature
NumberOfPairs()
Returns: Return type: int New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
-------------------------------------
Setter Method
Signature
NumberOfPairs(numberOfPairs)
Parameters: numberOfPairs (int) – New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
ParallelReinforcement¶
-
DuctReinforcementBuilder.
ParallelReinforcement
¶ Returns or sets the stock settings for parallel reinforcements
-------------------------------------
Getter Method
Signature
ParallelReinforcement()
Returns: Return type: NXOpen.Routing.PathStockBuilder
New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
-------------------------------------
Setter Method
Signature
ParallelReinforcement(parallelStockBuilder)
Parameters: parallelStockBuilder ( NXOpen.Routing.PathStockBuilder
) –New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
ParentDuct¶
-
DuctReinforcementBuilder.
ParentDuct
¶ Returns the duct that is to be reinforced.
-------------------------------------
Getter Method
Signature
ParentDuct()
Returns: Return type: NXOpen.Routing.SelectStock
New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
PathCurve¶
-
DuctReinforcementBuilder.
PathCurve
¶ Returns the path curve that is used to specify perpendicular reinforcement defining points.
-------------------------------------
Getter Method
Signature
PathCurve()
Returns: Return type: NXOpen.Curve
New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
PerpendicularReinforcement¶
-
DuctReinforcementBuilder.
PerpendicularReinforcement
¶ Returns or sets the stock settings for perpendicular reinforcements
-------------------------------------
Getter Method
Signature
PerpendicularReinforcement()
Returns: Return type: NXOpen.Routing.PathStockBuilder
New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
-------------------------------------
Setter Method
Signature
PerpendicularReinforcement(perpendicularStockBuilder)
Parameters: perpendicularStockBuilder ( NXOpen.Routing.PathStockBuilder
) –New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
ReinforcementType¶
-
DuctReinforcementBuilder.
ReinforcementType
¶ Returns or sets the type of reinforcement
-------------------------------------
Getter Method
Signature
ReinforcementType()
Returns: Return type: NXOpen.Routing.DuctReinforcementBuilderReinforcementTypes
New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
-------------------------------------
Setter Method
Signature
ReinforcementType(reinforcementType)
Parameters: reinforcementType ( NXOpen.Routing.DuctReinforcementBuilderReinforcementTypes
) –New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
SpacingExpression¶
-
DuctReinforcementBuilder.
SpacingExpression
¶ Returns the distance between each pair of reinforcement
-------------------------------------
Getter Method
Signature
SpacingExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
Method Detail¶
UpdatePathCurve¶
-
DuctReinforcementBuilder.
UpdatePathCurve
¶ The path curve that is used to specify perpendicular reinforcement defining points.
Signature
UpdatePathCurve()
New in version NX8.5.2.
License requirements: routing_hvac (“Routing HVAC”)
Validate¶
-
DuctReinforcementBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.