PathStockBuilder Class¶
-
class
NXOpen.Routing.
PathStockBuilder
¶ Bases:
NXOpen.Builder
Assigns stocks to segments based of users critiera and the current default stock.
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreatePathStockBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AssignStockMethod | Returns or sets the method to determine which stock to assign. |
DiameterValue | Returns or sets the diameter value to use for the Routing.PathStockBuilderAssignMethod.DiameterValue method of stock assignment. |
FlatOvalHeight | Returns the height value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.FlatOval < Routing.PathStockBuilderAssignMethod>` method of stock assignment. |
FlatOvalRotation | Returns the Width value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.FlatOval < Routing.PathStockBuilderAssignMethod>` method of stock assignment |
FlatOvalWidth | Returns the Width value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.FlatOval < Routing.PathStockBuilderAssignMethod>` method of stock assignment |
RectangularHeight | Returns the height value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.Rectangular < Routing.PathStockBuilderAssignMethod>` method of stock assignment. |
RectangularRotation | Returns the Width value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.Rectangular < Routing.PathStockBuilderAssignMethod>` method of stock assignment |
RectangularWidth | Returns the Width value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.Rectangular < Routing.PathStockBuilderAssignMethod>` method of stock assignment |
StartObject | Returns or sets the start object to use for the Routing.PathStockBuilderAssignMethod.FromStartObject method of stock assignment. |
StockType | Returns or sets the type of stock being assigned. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AssignStock | Assigns stock using the method defined by this stock builder object. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFlatOvalDimensions | Get the FlatOval height and width value to use for the FlatOval space reservation assignment |
GetObject | Returns the object currently being edited by this builder. |
GetParts | Get the parts to use for the :py:class:` Routing.PathStockBuilderAssignMethod.FromParts < Routing.PathStockBuilderAssignMethod>` method of stock assignment @return Part table parts to get stock characteristics. |
GetRectangularDimensions | Get the rectangular height and width value to use for the rectangular space reservation assignment |
GetSpecifiedStock | Returns the specified stock to use for the Routing.PathStockBuilderAssignMethod.SpecifiedStock method of stock assignment. |
SetFlatOvalDimensions | Set the FlatOval height and width value for the FlatOval space reservation assignment |
SetParts | Set the parts to use for the :py:class:` Routing.PathStockBuilderAssignMethod.FromParts < Routing.PathStockBuilderAssignMethod>` method of stock assignment |
SetRectangularDimensions | Set the rectangular height and width value for the rectangular space reservation assignment |
SetSelectedStock | Set the selected stock |
SetSpecifiedStock | Sets the specified stock to use for the Routing.PathStockBuilderAssignMethod.SpecifiedStock method of stock assignment. |
SettingsChanged | Notify the builder that the Routing preferred stock has been modified. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateExistingStock | Updates an existing routing stock with settings stored in the builder. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PathStockBuilderAssignMethod Enumeration | Determines how to choose which stock to assign. |
PathStockBuilderAssignStockType Enumeration | Determines the type of stock being assigned. |
Property Detail¶
AssignStockMethod¶
-
PathStockBuilder.
AssignStockMethod
¶ Returns or sets the method to determine which stock to assign.
-------------------------------------
Getter Method
Signature
AssignStockMethod()
Returns: Return type: NXOpen.Routing.PathStockBuilderAssignMethod
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AssignStockMethod(method)
Parameters: method ( NXOpen.Routing.PathStockBuilderAssignMethod
) –New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
DiameterValue¶
-
PathStockBuilder.
DiameterValue
¶ Returns or sets the diameter value to use for the
Routing.PathStockBuilderAssignMethod.DiameterValue
method of stock assignment.-------------------------------------
Getter Method
Signature
DiameterValue()
Returns: Return type: float New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
DiameterValue(val)
Parameters: val (float) – New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
FlatOvalHeight¶
-
PathStockBuilder.
FlatOvalHeight
¶ Returns the height value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.FlatOval < Routing.PathStockBuilderAssignMethod>` method of stock assignment.
-------------------------------------
Getter Method
Signature
FlatOvalHeight()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
FlatOvalRotation¶
-
PathStockBuilder.
FlatOvalRotation
¶ Returns the Width value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.FlatOval < Routing.PathStockBuilderAssignMethod>` method of stock assignment
-------------------------------------
Getter Method
Signature
FlatOvalRotation()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
FlatOvalWidth¶
-
PathStockBuilder.
FlatOvalWidth
¶ Returns the Width value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.FlatOval < Routing.PathStockBuilderAssignMethod>` method of stock assignment
-------------------------------------
Getter Method
Signature
FlatOvalWidth()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
RectangularHeight¶
-
PathStockBuilder.
RectangularHeight
¶ Returns the height value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.Rectangular < Routing.PathStockBuilderAssignMethod>` method of stock assignment.
-------------------------------------
Getter Method
Signature
RectangularHeight()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
RectangularRotation¶
-
PathStockBuilder.
RectangularRotation
¶ Returns the Width value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.Rectangular < Routing.PathStockBuilderAssignMethod>` method of stock assignment
-------------------------------------
Getter Method
Signature
RectangularRotation()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
RectangularWidth¶
-
PathStockBuilder.
RectangularWidth
¶ Returns the Width value to use for the :py:class:` Routing.PathStockBuilderAssignMethod.Rectangular < Routing.PathStockBuilderAssignMethod>` method of stock assignment
-------------------------------------
Getter Method
Signature
RectangularWidth()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
StartObject¶
-
PathStockBuilder.
StartObject
¶ Returns or sets the start object to use for the
Routing.PathStockBuilderAssignMethod.FromStartObject
method of stock assignment.-------------------------------------
Getter Method
Signature
StartObject()
Returns: Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
StartObject(startObject)
Parameters: startObject ( NXOpen.NXObject
) –New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
StockType¶
-
PathStockBuilder.
StockType
¶ Returns or sets the type of stock being assigned.
-------------------------------------
Getter Method
Signature
StockType()
Returns: Return type: NXOpen.Routing.PathStockBuilderAssignStockType
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
StockType(stockType)
Parameters: stockType ( NXOpen.Routing.PathStockBuilderAssignStockType
) –New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
AssignStock¶
-
PathStockBuilder.
AssignStock
¶ Assigns stock using the method defined by this stock builder object.
Signature
AssignStock(segments)
Parameters: segments (list of NXOpen.Routing.ISegment
) –New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
GetFlatOvalDimensions¶
-
PathStockBuilder.
GetFlatOvalDimensions
¶ Get the FlatOval height and width value to use for the FlatOval space reservation assignment
Signature
GetFlatOvalDimensions()
Returns: a tuple Return type: A tuple consisting of (height, width). height is a float. width is a float. New in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
GetParts¶
-
PathStockBuilder.
GetParts
¶ Get the parts to use for the :py:class:` Routing.PathStockBuilderAssignMethod.FromParts < Routing.PathStockBuilderAssignMethod>` method of stock assignment
Signature
GetParts()
Returns: Part table parts to get stock characteristics.
Return type: list of NXOpen.Assemblies.Component
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
GetRectangularDimensions¶
-
PathStockBuilder.
GetRectangularDimensions
¶ Get the rectangular height and width value to use for the rectangular space reservation assignment
Signature
GetRectangularDimensions()
Returns: a tuple Return type: A tuple consisting of (height, width). height is a float. width is a float. New in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
GetSpecifiedStock¶
-
PathStockBuilder.
GetSpecifiedStock
¶ Returns the specified stock to use for the
Routing.PathStockBuilderAssignMethod.SpecifiedStock
method of stock assignment.Signature
GetSpecifiedStock()
Returns: Characteristic list used to find the appropriate Routing.StockData
for building the stock. SeeRouting.StockDataCollection.CreateStockData
. :rtype:NXOpen.Routing.CharacteristicList
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
SetFlatOvalDimensions¶
-
PathStockBuilder.
SetFlatOvalDimensions
¶ Set the FlatOval height and width value for the FlatOval space reservation assignment
Signature
SetFlatOvalDimensions(height, width)
Parameters: - height (float) –
- width (float) –
New in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
SetParts¶
-
PathStockBuilder.
SetParts
¶ Set the parts to use for the :py:class:` Routing.PathStockBuilderAssignMethod.FromParts < Routing.PathStockBuilderAssignMethod>` method of stock assignment
Signature
SetParts(parts)
Parameters: parts (list of NXOpen.Assemblies.Component
) – Part table parts to get stock characteristics.New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
SetRectangularDimensions¶
-
PathStockBuilder.
SetRectangularDimensions
¶ Set the rectangular height and width value for the rectangular space reservation assignment
Signature
SetRectangularDimensions(height, width)
Parameters: - height (float) –
- width (float) –
New in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
SetSelectedStock¶
-
PathStockBuilder.
SetSelectedStock
¶ Set the selected stock
Signature
SetSelectedStock(stock)
Parameters: stock ( NXOpen.Routing.Stock
) – Selected StockNew in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
SetSpecifiedStock¶
-
PathStockBuilder.
SetSpecifiedStock
¶ Overloaded method SetSpecifiedStock
SetSpecifiedStock(stockPart)
SetSpecifiedStock(stockPart, appliedCharx)
-------------------------------------
Sets the specified stock to use for the
Routing.PathStockBuilderAssignMethod.SpecifiedStock
method of stock assignment.Signature
SetSpecifiedStock(stockPart)
Parameters: stockPart ( NXOpen.Routing.CharacteristicList
) – Characteristic list used to find the appropriateRouting.StockData
for building the stock. SeeRouting.StockDataCollection.CreateStockData
.New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Sets the specified stock and applied characteristics to use for the
Routing.PathStockBuilderAssignMethod.SpecifiedStock
method of stock assignment.Signature
SetSpecifiedStock(stockPart, appliedCharx)
Parameters: - stockPart (
NXOpen.Routing.CharacteristicList
) – Characteristic list used to find the appropriateRouting.StockData
for building the stock. SeeRouting.StockDataCollection.CreateStockData
. - appliedCharx (
NXOpen.Routing.CharacteristicList
) – Applied characteristics for the specified stock.
New in version NX6.0.4.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
SettingsChanged¶
-
PathStockBuilder.
SettingsChanged
¶ Notify the builder that the Routing preferred stock has been modified.
This updates the builder so that it now uses the new preferred stock do determine which stock to assign.
Signature
SettingsChanged()
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
UpdateExistingStock¶
-
PathStockBuilder.
UpdateExistingStock
¶ Updates an existing routing stock with settings stored in the builder.
Signature
UpdateExistingStock(existingStock)
Parameters: existingStock ( NXOpen.Routing.Stock
) – Existing StockNew in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
PathStockBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.