StockCollection Class¶
-
class
NXOpen.Routing.
StockCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.Stock
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
AddStock | Creates stock on the given segments. |
ConvertToStockAsComponents | Converts a part file from Legacy Stock into Stock as Components. |
CreateStock | Creates a NXOpen.Routing.Stock object. |
GetComponentStock | Returns the NXOpen.Routing.Stock that controls the given component. |
RemoveAllFillerStocks | Removes all filler stocks from the input set of segments. |
RemoveStock | Removes all stocks (excluding flexed stocks) from the input set of segments. |
ResetReferenceStock | Resets the reference NXOpen.Routing.Stock information to None. |
SetAttachedStockLength | Set the length of the NXOpen.Routing.Stock to which a NXOpen.Assemblies.Component object is attached. |
SetReferenceStockFromObject | Sets the reference NXOpen.Routing.Stock information based on the NXOpen.Routing.Stock associated with this object. |
UpdateBundleStockForFiller | Update the bundle stock if the NXOpen.Routing.Filler stock is created underneath it. |
Method Detail¶
AddStock¶
-
StockCollection.
AddStock
¶ Overloaded method AddStock
AddStock(stockPart, dataCharx, segments, routeLevel)
AddStock(stockPart, dataCharx, segments, routeLevel, isSpaceReservation)
AddStock(stockPart, dataCharx, segments, routeLevel, isSpaceReservation, anchorName)
-------------------------------------
Creates stock on the given segments. The segments do not need to be in order, and don’t necessarily have to form a single path.
Signature
AddStock(stockPart, dataCharx, segments, routeLevel)
Parameters: - stockPart (
NXOpen.Routing.CharacteristicList
) – Characteristic list used to find the appropriateNXOpen.Routing.StockData
for building the stock. SeeRouting.StockDataCollection.CreateStockData
. - dataCharx (
NXOpen.Routing.CharacteristicList
) – The list of optional and required characteristics to apply to the new stock. - segments (list of
NXOpen.Routing.ISegment
) – - routeLevel (str) – Routing level. NOTE: The full Unicode character set is not supported for this parameter.
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates normal or space reservation stock on the given segments. The segments do not need to be in order, and don’t necessarily have to form a single path.
Signature
AddStock(stockPart, dataCharx, segments, routeLevel, isSpaceReservation)
Parameters: - stockPart (
NXOpen.Routing.CharacteristicList
) – Characteristic list used to find the appropriateNXOpen.Routing.StockData
for building the stock. SeeRouting.StockDataCollection.CreateStockData
. - dataCharx (
NXOpen.Routing.CharacteristicList
) – The list of optional and required characteristics to apply to the new stock. - segments (list of
NXOpen.Routing.ISegment
) – - routeLevel (str) – Routing level. NOTE: The full Unicode character set is not supported for this parameter.
- isSpaceReservation (bool) – TRUE to create Space Reservation stock, FALSE to create normal stock
Returns: Array of stocks created
Return type: list of
NXOpen.Routing.Stock
New in version NX7.5.2.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates normal or space reservation stock on the given segments. The segments do not need to be in order, and don’t necessarily have to form a single path.
Signature
AddStock(stockPart, dataCharx, segments, routeLevel, isSpaceReservation, anchorName)
Parameters: - stockPart (
NXOpen.Routing.CharacteristicList
) – Characteristic list used to find the appropriateNXOpen.Routing.StockData
for building the stock. SeeRouting.StockDataCollection.CreateStockData
. - dataCharx (
NXOpen.Routing.CharacteristicList
) – The list of optional and required characteristics to apply to the new stock. - segments (list of
NXOpen.Routing.ISegment
) – - routeLevel (str) – Routing level. NOTE: The full Unicode character set is not supported for this parameter.
- isSpaceReservation (bool) – TRUE to create Space Reservation stock, FALSE to create normal stock
- anchorName (str) – Name of the anchor to use. NOTE: The full Unicode character set is not supported for this parameter.
Returns: Array of stocks created
Return type: list of
NXOpen.Routing.Stock
New in version NX7.5.2.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
ConvertToStockAsComponents¶
-
StockCollection.
ConvertToStockAsComponents
¶ Overloaded method ConvertToStockAsComponents
ConvertToStockAsComponents(nameType)
ConvertToStockAsComponents(convertSpaceReservartion, nameType)
-------------------------------------
Converts a part file from Legacy Stock into Stock as Components. Converts all stocks whose use is
NXOpen.Routing.StockUse.LegacyStock
intoNXOpen.Routing.StockUse.StockAsComponent
stocks by creating components for each stock. After calling this routine, all new stocks in this part will have components associated with them.Signature
ConvertToStockAsComponents(nameType)
Parameters: nameType ( NXOpen.Routing.ComponentName
) – Naming scheme to use for components. Calls ??? on each new stock component if input isRoutingComponentName.Permanent
.New in version NX4.0.0.
Deprecated since version NX8.0.0: Use
Routing.StockCollection.ConvertToStockAsComponents
instead.License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Converts a part file from Legacy Stock into Stock as Components. Converts all stocks whose use is
NXOpen.Routing.StockUse.LegacyStock
intoNXOpen.Routing.StockUse.StockAsComponent
stocks by creating components for each stock. After calling this routine, all new stocks in this part will have components associated with them.Signature
ConvertToStockAsComponents(convertSpaceReservartion, nameType)
Parameters: - convertSpaceReservartion (bool) – If true, convert Space Reservation as Components
- nameType (
NXOpen.Routing.ComponentName
) – Naming scheme to use for components. Calls ??? on each new stock component if input isRoutingComponentName.Permanent
.
New in version NX7.5.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
CreateStock¶
-
StockCollection.
CreateStock
¶ Creates a
NXOpen.Routing.Stock
object.Signature
CreateStock(stockData, anchor, crossSection, segments)
Parameters: - stockData (
NXOpen.Routing.StockData
) – TheNXOpen.Routing.StockData
that defines the stock - anchor (
NXOpen.Routing.Anchor
) – TheNXOpen.Routing.Anchor
from the inputNXOpen.Routing.StockData
to use, None is allowed for no anchor. - crossSection (
NXOpen.Routing.CrossSection
) – TheNXOpen.Routing.CrossSection
from the inputNXOpen.Routing.StockData
to use, None is not allowed. - segments (list of
NXOpen.Routing.ISegment
) – The array ofNXOpen.Routing.ISegment
curves that the stock must cover.
Returns: The resulting array of newly created
NXOpen.Routing.Stock
objects. :rtype: list of
NXOpen.Routing.Stock
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
- stockData (
GetComponentStock¶
-
StockCollection.
GetComponentStock
¶ Returns the
NXOpen.Routing.Stock
that controls the given component.Only returns a
NXOpen.Routing.Stock
if the input component is a component created by a Stock as Components stock object.Signature
GetComponentStock(component)
Parameters: component ( NXOpen.Assemblies.Component
) –Returns: Returns None if the input component is not controlled by a
NXOpen.Routing.Stock
:rtype:NXOpen.Routing.Stock
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
RemoveAllFillerStocks¶
-
StockCollection.
RemoveAllFillerStocks
¶ Removes all filler stocks from the input set of segments.
Signature
RemoveAllFillerStocks(segments)
Parameters: segments (list of NXOpen.Routing.ISegment
) –New in version NX5.0.4.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
RemoveStock¶
-
StockCollection.
RemoveStock
¶ Removes all stocks (excluding flexed stocks) from the input set of segments.
Signature
RemoveStock(segments)
Parameters: segments (list of NXOpen.Routing.ISegment
) –New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
ResetReferenceStock¶
-
StockCollection.
ResetReferenceStock
¶ Resets the reference
NXOpen.Routing.Stock
information to None.The information attributes are rotation, twist, negate, flip, port and anchor. They determine the default creation options for the new stock. This information is used during path creation.
Signature
ResetReferenceStock()
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
SetAttachedStockLength¶
-
StockCollection.
SetAttachedStockLength
¶ Set the length of the
NXOpen.Routing.Stock
to which aNXOpen.Assemblies.Component
object is attached.Signature
SetAttachedStockLength(partOcc)
Parameters: partOcc ( NXOpen.Assemblies.Component
) –New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
SetReferenceStockFromObject¶
-
StockCollection.
SetReferenceStockFromObject
¶ Sets the reference
NXOpen.Routing.Stock
information based on theNXOpen.Routing.Stock
associated with this object.Signature
SetReferenceStockFromObject(object)
Parameters: object ( NXOpen.NXObject
) –New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
UpdateBundleStockForFiller¶
-
StockCollection.
UpdateBundleStockForFiller
¶ Update the bundle stock if the
NXOpen.Routing.Filler
stock is created underneath it.Signature
UpdateBundleStockForFiller(segments)
Parameters: segments (list of NXOpen.Routing.ISegment
) –New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)