HandrailBuilder Class¶
-
class
NXOpen.Routing.
HandrailBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Routing.HandrailBuilder
Creates a handrail from a selected point.The handrail is created by optionally placing a post depending on the post type followed by placing the rails across the route control points corresponding to the posts.
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateHandrailBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AutoCloseOption | Returns or sets an option to automatically close the handrail |
HasHorizontalRails | Returns or sets an option to create horizontal rail stock |
PostType | Returns or sets the type of post: Start, Intermediate, None, End |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
PlaceHandrail | Creates a handrail post, horizontal railings assembly components and places them in the appropriate orientation. |
ReverseLastPost | Reverses the orientation of the last placed post |
SetHandrailPartCharx | Sets the handrail part characteristics |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HandrailBuilderPostTypes Enumeration | The post type: Start, Intermediate, None, End. |
Property Detail¶
AutoCloseOption¶
-
HandrailBuilder.
AutoCloseOption
¶ Returns or sets an option to automatically close the handrail
-------------------------------------
Getter Method
Signature
AutoCloseOption()
Returns: Return type: bool New in version NX8.5.0.
License requirements: routing_platform (“Routing Platform”)
-------------------------------------
Setter Method
Signature
AutoCloseOption(autoClose)
Parameters: autoClose (bool) – New in version NX8.5.0.
License requirements: routing_platform (“Routing Platform”)
HasHorizontalRails¶
-
HandrailBuilder.
HasHorizontalRails
¶ Returns or sets an option to create horizontal rail stock
-------------------------------------
Getter Method
Signature
HasHorizontalRails()
Returns: Return type: bool New in version NX8.5.0.
License requirements: routing_platform (“Routing Platform”)
-------------------------------------
Setter Method
Signature
HasHorizontalRails(railOption)
Parameters: railOption (bool) – New in version NX8.5.0.
License requirements: routing_platform (“Routing Platform”)
PostType¶
-
HandrailBuilder.
PostType
¶ Returns or sets the type of post: Start, Intermediate, None, End
-------------------------------------
Getter Method
Signature
PostType()
Returns: Return type: NXOpen.Routing.HandrailBuilderPostTypes
New in version NX8.5.0.
License requirements: routing_platform (“Routing Platform”)
-------------------------------------
Setter Method
Signature
PostType(postType)
Parameters: postType ( NXOpen.Routing.HandrailBuilderPostTypes
) –New in version NX8.5.0.
License requirements: routing_platform (“Routing Platform”)
Method Detail¶
PlaceHandrail¶
-
HandrailBuilder.
PlaceHandrail
¶ Creates a handrail post, horizontal railings assembly components and places them in the appropriate orientation.
Signature
PlaceHandrail(postLocation)
Parameters: postLocation ( NXOpen.Point3d
) – The point where the handrail is to be placedNew in version NX8.5.0.
License requirements: routing_platform (“Routing Platform”)
ReverseLastPost¶
-
HandrailBuilder.
ReverseLastPost
¶ Reverses the orientation of the last placed post
Signature
ReverseLastPost()
New in version NX8.5.0.
License requirements: routing_platform (“Routing Platform”)
SetHandrailPartCharx¶
-
HandrailBuilder.
SetHandrailPartCharx
¶ Sets the handrail part characteristics
Signature
SetHandrailPartCharx(partCharx)
Parameters: partCharx ( NXOpen.Routing.CharacteristicList
) – The characteristics to use for the handrail postsNew in version NX8.5.0.
License requirements: routing_platform (“Routing Platform”)
Validate¶
-
HandrailBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.