FillerStockBuilder Class¶
-
class
NXOpen.Routing.
FillerStockBuilder
¶ Bases:
NXOpen.Builder
Creates Filler stock on selected Segments.
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateFillerStockBuilder
Default values.
Property Value RemoveExistingStock 0 StockSettings.AssignStockMethod SpecifiedStock New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
RemoveExistingStock | Returns or sets the remove existing stock flag. |
RouteSelection | Returns the route selection which allows selection of routing objects |
StockSettings | Returns or sets the stock settings for creating filler stock. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
RemoveExistingStock¶
-
FillerStockBuilder.
RemoveExistingStock
¶ Returns or sets the remove existing stock flag.
If set to TRUE the existing stock on the path will be removed when assigning new stock.
-------------------------------------
Getter Method
Signature
RemoveExistingStock()
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
RemoveExistingStock(removeStock)
Parameters: removeStock (bool) – New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
RouteSelection¶
-
FillerStockBuilder.
RouteSelection
¶ Returns the route selection which allows selection of routing objects
-------------------------------------
Getter Method
Signature
RouteSelection()
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
StockSettings¶
-
FillerStockBuilder.
StockSettings
¶ Returns or sets the stock settings for creating filler stock.
-------------------------------------
Getter Method
Signature
StockSettings()
Returns: Return type: NXOpen.Routing.PathStockBuilder
New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
StockSettings(stockBuilder)
Parameters: stockBuilder ( NXOpen.Routing.PathStockBuilder
) –New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
Method Detail¶
Validate¶
-
FillerStockBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.