Overstock Class¶
-
class
NXOpen.Routing.
Overstock
¶ Bases:
NXOpen.Routing.Stock
Represents an
NXOpen.Routing.Overstock
object.Creator not available in KF.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
NegateOffsetsFlag | Returns or sets the negate offsets flag of this NXOpen.Routing.Stock . |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddSegments | Adds new segments to this object. |
AlignStock | Align stock to new rotation vector. |
ColorBodies | Colors the solid bodies of the stock based on the COLOR characteristic specified in the NXOpen.Routing.StockData of the stock. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteCharacterstics | Removes the input list of characteristics from this object. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
EnableFeatures | Makes the stock featurable by generating a sweep feature over every segment of the stock, with a boolean feature uniting all of the sweeps to form a single body. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAnchor | Gets the NXOpen.Routing.Anchor that currently modifies the profile for the stock. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCharacteristics | Get all of the characteristics values on the this object. |
GetComponent | Returns the NXOpen.Assemblies.Component created and controlled by the stock for a Stock as Components stock. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetCoveredStocks | Get the stocks covering this NXOpen.Routing.Overstock . |
GetCrossSection | Gets the NXOpen.Routing.CrossSection that currently defines the profile for the stock. |
GetDestinationCharacteristics | Returns the destination characteristics from the input object. |
GetFeatures | Returns the sweep features that are created and controlled by this object. |
GetFlippedStatus | Gets whether or not the profile is flipped. |
GetGapDistance | Get the gap distance for this NXOpen.Routing.Overstock . |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerCharacteristic | Get the value of an integer characteristic associated with the input name. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNameStatus | Returns whether or not the component associated with a Stock as Components Stock has a permanent or temporary name. |
GetNumberOfWraps | Returns the number of wraps for this NXOpen.Routing.Overstock . |
GetOriginalLength | Returns the original length for a stock that has been deformed (it’s use is RoutingStockUse.Deformed ). |
GetOverstockCreationMethod | Returns the creation method of this NXOpen.Routing.Overstock . |
GetOverstockSegments | Returns the segments over which this NXOpen.Routing.Overstock is applied. |
GetOverstockType | Returns the type of overstock. |
GetPercentageOverlap | Get the overlap percentage of this NXOpen.Routing.Overstock . |
GetPorts | Returns the NXOpen.Routing.StockPort at each end of the stock. |
GetProfileEnd | Gets the end that defines profile. |
GetRealAttribute | Gets a real attribute by title. |
GetRealCharacteristic | Get the value of a real characteristic associated with the input name. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetRotationAngle | Gets the rotation angle applied to the profile. |
GetSegments | Gets the segments that the NXOpen.Routing.Stock object is placed on top of. |
GetStockData | Gets the NXOpen.Routing.StockData . |
GetStockStyle | Gets the NXOpen.Routing.StockStyle of the NXOpen.Routing.Stock . |
GetStockUse | Returns the use of the stock. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringCharacteristic | Get the value of a string characteristic associated with the input name. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetThickness | Get the thickness of this NXOpen.Routing.Overstock . |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetTwistAngle | Gets the twist angle applied to the profile. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetWidth | Get the width of this NXOpen.Routing.Overstock . |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Prints a representation of this object to the system log file. | |
RemoveSegments | Removes segments from this object. |
RenameStockComponent | Renames the stock component part with given name |
SetAnchor | Sets the NXOpen.Routing.Anchor . |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCharacteristic | Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. |
SetCharacteristics | Set all of the characteristics values on this object. |
SetCrossSection | Sets the NXOpen.Routing.CrossSection . |
SetFlippedStatus | Sets whether or not the profile is flipped. |
SetName | Sets the custom name of the object. |
SetProfileEnd | Sets the end that defines profile. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetRotationAngle | Sets the rotation angle applied to the profile. |
SetStockData | Sets the NXOpen.Routing.StockData . |
SetStockStyle | Sets the NXOpen.Routing.StockStyle of the NXOpen.Routing.Stock . |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetTwistAngle | Sets the twist angle applied to the profile. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SyncComponentAttrs | Set the characteristics of the given stock’s component so that it has the same characteristics as the NXOpen.Routing.Stock and its stock data. |
Property Detail¶
IsOccurrence¶
-
Overstock.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Overstock.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Overstock.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Overstock.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Overstock.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Overstock.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
DeleteCharacterstics¶
-
Overstock.
DeleteCharacterstics
¶ Removes the input list of characteristics from this object.
Signature
DeleteCharacterstics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FindObject¶
-
Overstock.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetCharacteristics¶
-
Overstock.
GetCharacteristics
¶ Get all of the characteristics values on the this object.
Signature
GetCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetCoveredStocks¶
-
Overstock.
GetCoveredStocks
¶ Get the stocks covering this
NXOpen.Routing.Overstock
.Signature
GetCoveredStocks()
Returns: Return type: list of NXOpen.Routing.Stock
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
GetDestinationCharacteristics¶
-
Overstock.
GetDestinationCharacteristics
¶ Returns the destination characteristics from the input object.
Retrieves the description of which destination characteristics to read from the application view and then reads those destination characteristics from the object
- Ports: Reads characteristics from the port.
- RCPs: Attempts to find a port at the RCP, reads characteristics from
the port if it exists, otherwise reads from the stock associated with the rcp.
- Segments: Reads characteristics from the stock associated with the segment.
- Components: Reads characteristics directly from the component.
- Stock: Reads characteristics from the stock or from the stock’s data.
Signature
GetDestinationCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetGapDistance¶
-
Overstock.
GetGapDistance
¶ Get the gap distance for this
NXOpen.Routing.Overstock
.Signature
GetGapDistance()
Returns: Return type: NXOpen.Scalar
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
GetIntegerCharacteristic¶
-
Overstock.
GetIntegerCharacteristic
¶ Get the value of an integer characteristic associated with the input name.
Signature
GetIntegerCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: int New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetNumberOfWraps¶
-
Overstock.
GetNumberOfWraps
¶ Returns the number of wraps for this
NXOpen.Routing.Overstock
.Signature
GetNumberOfWraps()
Returns: Return type: NXOpen.Scalar
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
GetOverstockCreationMethod¶
-
Overstock.
GetOverstockCreationMethod
¶ Returns the creation method of this
NXOpen.Routing.Overstock
.Signature
GetOverstockCreationMethod()
Returns: Return type: NXOpen.Routing.CreationMethod
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
GetOverstockSegments¶
-
Overstock.
GetOverstockSegments
¶ Returns the segments over which this
NXOpen.Routing.Overstock
is applied.Signature
GetOverstockSegments()
Returns: Return type: list of NXOpen.Curve
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
GetOverstockType¶
-
Overstock.
GetOverstockType
¶ Returns the type of overstock.
Possible types are wrapped, sleeved, flagged and an overstock with fixed cross section.
Signature
GetOverstockType()
Returns: Return type: NXOpen.Routing.Type
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
GetPercentageOverlap¶
-
Overstock.
GetPercentageOverlap
¶ Get the overlap percentage of this
NXOpen.Routing.Overstock
.Signature
GetPercentageOverlap()
Returns: Return type: NXOpen.Scalar
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
GetRealCharacteristic¶
-
Overstock.
GetRealCharacteristic
¶ Get the value of a real characteristic associated with the input name.
Signature
GetRealCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetStringCharacteristic¶
-
Overstock.
GetStringCharacteristic
¶ Get the value of a string characteristic associated with the input name.
Signature
GetStringCharacteristic(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetThickness¶
-
Overstock.
GetThickness
¶ Get the thickness of this
NXOpen.Routing.Overstock
.Signature
GetThickness()
Returns: Return type: NXOpen.Scalar
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
GetWidth¶
-
Overstock.
GetWidth
¶ Get the width of this
NXOpen.Routing.Overstock
.Signature
GetWidth()
Returns: Return type: NXOpen.Scalar
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”) OR routing_harness (“Routing Harness”) OR routing_cabling (“Routing Cabling”) OR routing_pipetube (“Routing Piping and Tubing”) OR routing_hvac (“Routing HVAC”) OR routing_platform (“Routing Platform”) OR routing_pid (“Routing PID”)
Print¶
-
Overstock.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetCharacteristic¶
-
Overstock.
SetCharacteristic
¶ Overloaded method SetCharacteristic
SetCharacteristic(name, value)
SetCharacteristic(name, value)
SetCharacteristic(name, value)
-------------------------------------
Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to integer if it’s type is not integer.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (int) –
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an real characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to real if it’s type is not real.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (float) –
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an string characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to string if it’s type is not string.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristics¶
-
Overstock.
SetCharacteristics
¶ Set all of the characteristics values on this object.
Signature
SetCharacteristics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetName¶
-
Overstock.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.