OffsetPathCollection Class¶
-
class
NXOpen.Routing.
OffsetPathCollection
¶ Bases:
object
The Routing OffsetPath object is a list of segments in a route.
It also contains the beginning and ending control point for the path.
To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
ConvertOffsetPaths | Converts an offset path into NXOpen.Positioning.Constraint objects applied to the copied routing objects. |
CreateCircularOffsetPath | Creates a circular offset path. |
CreateRectangularOffsetPath | Creates a rectangular offset path. |
Enumerations¶
OffsetPathCollectionBendType Enumeration | Bend types for offset path creation |
Method Detail¶
ConvertOffsetPaths¶
-
OffsetPathCollection.
ConvertOffsetPaths
¶ Converts an offset path into
NXOpen.Positioning.Constraint
objects applied to the copied routing objects.Converts the input master offset path as well as all of the children offset paths of the input master offset path.
The
NXOpen.Routing.OffsetPath
is incompatible with segments created using theNXOpen.Routing.SegmentManager.CreateConstrainedSegment
or to any segments that haveNXOpen.Positioning.Constraint
objects applied to them. This routine makes the path parallel and associative to each other using constraints rather than theNXOpen.Routing.OffsetPath
objects. The converted offset path objects are logged for delete, the next call toNXOpen.Update.DoUpdate
will delete the offset path objects.Signature
ConvertOffsetPaths(masterOffsetPath)
Parameters: masterOffsetPath ( NXOpen.Routing.OffsetPath
) –New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
CreateCircularOffsetPath¶
-
OffsetPathCollection.
CreateCircularOffsetPath
¶ Creates a circular offset path.
Signature
CreateCircularOffsetPath(segments, allStock, specStocks, maintainStock, copyBendCorners, maintain, useMinimumBendRatio, minimumBendRatio, minimumBendRadius, deleteAllDuplicates, createAssociativePaths, patternXVector, patternYVector, patternAxisEndPoint, patternStartAngle, radialOffset, nPaths, totalAngle)
Parameters: - segments (list of
NXOpen.Routing.ISegment
) – The list of segments to be associated with the offset path - allStock (bool) –
- specStocks (list of
NXOpen.Routing.Stock
) – - maintainStock (bool) – if TRUE: Maintain stock on paths
- copyBendCorners (bool) – if TRUE: Copy the bend corners
- maintain (
NXOpen.Routing.OffsetPathCollectionBendType
) – Maintain radius or center - useMinimumBendRatio (bool) – if TRUE: Use Ratio to Stock Diameter
- minimumBendRatio (float) – Minimum Bend Ratio
- minimumBendRadius (float) – Minimum Bend Radius
- deleteAllDuplicates (bool) – if TRUE: Delete all duplicate paths
- createAssociativePaths (bool) – if TRUE: Create associative paths
- patternXVector (
NXOpen.Vector3d
) – X vector to set the pattern reference axis - patternYVector (
NXOpen.Vector3d
) – Y vector to set the pattern reference axis - patternAxisEndPoint (
NXOpen.Point3d
) – Point to set the pattern reference axis direction if NULL: Computes reference axis using heuristics - patternStartAngle (float) – Start angle of the point
- radialOffset (float) – Offset distance
- nPaths (int) – Number of paths
- totalAngle (float) – Total angle
Returns: a tuple
Return type: A tuple consisting of (masterOffsetPath, slavePathsCreated). masterOffsetPath is a
NXOpen.Routing.OffsetPath
. The created master offset path slavePathsCreated is a list ofNXOpen.Routing.OffsetPath
. The created slave offset pathsNew in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
- segments (list of
CreateRectangularOffsetPath¶
-
OffsetPathCollection.
CreateRectangularOffsetPath
¶ Creates a rectangular offset path.
Signature
CreateRectangularOffsetPath(segments, allStock, specStocks, maintainStock, copyBendCorners, maintain, useMinimumBendRatio, minimumBendRatio, minimumBendRadius, deleteAllDuplicates, createAssociativePaths, patternXVector, patternYVector, patternAxisEndPoint, patternStartAngle, rowOffset, columnOffset, nRows, nColumns, masterRow, masterColumn)
Parameters: - segments (list of
NXOpen.Routing.ISegment
) – The list of segments to be associated with the offset path - allStock (bool) –
- specStocks (list of
NXOpen.Routing.Stock
) – - maintainStock (bool) – if TRUE: Maintain stock on paths
- copyBendCorners (bool) – if TRUE: Copy the bend corners
- maintain (
NXOpen.Routing.OffsetPathCollectionBendType
) – Maintain radius or center - useMinimumBendRatio (bool) – if TRUE: Use Ratio to Stock Diameter
- minimumBendRatio (float) – Minimum Bend Ratio
- minimumBendRadius (float) – Minimum Bend Radius
- deleteAllDuplicates (bool) – if TRUE: Delete all duplicate paths
- createAssociativePaths (bool) – if TRUE: Create associative paths
- patternXVector (
NXOpen.Vector3d
) – X vector to set the pattern reference axis - patternYVector (
NXOpen.Vector3d
) – Y vector to set the pattern reference axis - patternAxisEndPoint (
NXOpen.Point3d
) – Point to set the pattern reference axis direction if NULL: Computes reference axis using heuristics - patternStartAngle (float) – Start angle of the pattern
- rowOffset (float) – Offset distance along the row
- columnOffset (float) – Offset distance along the column
- nRows (int) – Number of rows
- nColumns (int) – Number of columns
- masterRow (int) – Row of the master path
- masterColumn (int) – Column of the master path
Returns: a tuple
Return type: A tuple consisting of (masterOffsetPath, slavePathsCreated). masterOffsetPath is a
NXOpen.Routing.OffsetPath
. The created master offset path slavePathsCreated is a list ofNXOpen.Routing.OffsetPath
. The created slave offset pathsNew in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
- segments (list of