SegmentManager Class¶
-
class
NXOpen.Routing.
SegmentManager
¶ Bases:
object
Contains the type of the routing part as well as the Collection objects for creating/iterating over routing objects.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateConstrainedSegment | Creates a constrained line NXOpen.Routing.ISegment object with input NXOpen.Routing.ControlPoint as ends. |
CreateHealPath | Creates a new empty NXOpen.Routing.HealPath object that can be used as an input to NXOpen.Routing.SegmentManager.CreateHealSpline . |
CreateHealSpline | Creates a spline NXOpen.Routing.ISegment object with input NXOpen.Routing.ControlPoint as ends. |
CreateSegment | Creates a NXOpen.Routing.ISegment object following a curve. |
ModelTerminals | Models spline paths to to specified terminals. |
ProcessBuiltInPaths | Create segments of NXOpen.Routing.BuiltInPath objects present in this NXOpen.Assemblies.Component object. |
SetFollowCurve | Set segment follow curve. |
SimplifySegments | Combine segments that are collinear and whose intermediate RCPs do not branch |
Subdivide | Subdivide a routing path segment |
UnmodelTerminals | Un-model terminals and update connection list routes for specified terminal ports. |
Enumerations¶
SegmentManagerSubdivideSpacing Enumeration | Specifies spacing option for subdivide segment. |
Structs¶
SegmentManagerSubdivideOption_Struct Struct | Contains subdivide segment method information. |
Method Detail¶
CreateConstrainedSegment¶
-
SegmentManager.
CreateConstrainedSegment
¶ Creates a constrained line
NXOpen.Routing.ISegment
object with inputNXOpen.Routing.ControlPoint
as ends.Only use this method when building segments in a part that use
NXOpen.Positioning.Constraint
objects to constraint components and geometry. This is a new method for creating segments in NX5 and should be used instead ofNXOpen.Routing.SegmentManager.CreateSegment
for all line segments.Signature
CreateConstrainedSegment(startRcp, endRcp)
Parameters: - startRcp (
NXOpen.Routing.ControlPoint
) – StartNXOpen.Routing.ControlPoint
of the segment - endRcp (
NXOpen.Routing.ControlPoint
) – EndNXOpen.Routing.ControlPoint
of the segment
Returns: Created segment
Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
- startRcp (
CreateHealPath¶
-
SegmentManager.
CreateHealPath
¶ Creates a new empty
NXOpen.Routing.HealPath
object that can be used as an input toNXOpen.Routing.SegmentManager.CreateHealSpline
.Signature
CreateHealPath()
Returns: Return type: NXOpen.Routing.HealPath
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
CreateHealSpline¶
-
SegmentManager.
CreateHealSpline
¶ Creates a spline
NXOpen.Routing.ISegment
object with inputNXOpen.Routing.ControlPoint
as ends.Signature
CreateHealSpline(startObject, endObject, healPath)
Parameters: - startObject (
NXOpen.DisplayableObject
) – StartNXOpen.DisplayableObject
of the segment, ideally it should beNXOpen.Routing.Port
- endObject (
NXOpen.DisplayableObject
) – EndNXOpen.DisplayableObject
of the segment, ideally it should beNXOpen.Routing.Port
- healPath (
NXOpen.Routing.HealPath
) –
Returns: Created segment
Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
- startObject (
CreateSegment¶
-
SegmentManager.
CreateSegment
¶ Overloaded method CreateSegment
CreateSegment(followCurve, startRcp, endRcp, userDefined)
CreateSegment(startRcp, endRcp)
-------------------------------------
Creates a
NXOpen.Routing.ISegment
object following a curve.Signature
CreateSegment(followCurve, startRcp, endRcp, userDefined)
Parameters: - followCurve (
NXOpen.Curve
) – Curve to follow - startRcp (
NXOpen.Routing.ControlPoint
) – StartNXOpen.Routing.ControlPoint
of the segment - endRcp (
NXOpen.Routing.ControlPoint
) – EndNXOpen.Routing.ControlPoint
of the segment - userDefined (
NXOpen.Routing.UserDefined
) – Is segment user defined?
Returns: Created segment
Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a line
NXOpen.Routing.ISegment
object with inputNXOpen.Routing.ControlPoint
as ends.Signature
CreateSegment(startRcp, endRcp)
Parameters: - startRcp (
NXOpen.Routing.ControlPoint
) – StartNXOpen.Routing.ControlPoint
of the segment - endRcp (
NXOpen.Routing.ControlPoint
) – EndNXOpen.Routing.ControlPoint
of the segment
Returns: Created segment
Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
ModelTerminals¶
-
SegmentManager.
ModelTerminals
¶ Models spline paths to to specified terminals.
Updates connection list to reflect changes to wire lengths of referencing connections.
Signature
ModelTerminals(multiPort, cutBackLength, extensionString, overrideCharx, terminalPorts)
Parameters: - multiPort (
NXOpen.Routing.Port
) – MultiPort whose terminals are modeled - cutBackLength (float) – Length of cut back path connected to multiport.
- extensionString (str) – Length of terminal segments which extends parallel to terminal ports NOTE: The full Unicode character set is not supported for this parameter.
- overrideCharx (bool) – if TRUE: extension_string determines all terminal extensions
- terminalPorts (list of
NXOpen.Routing.Port
) – Terminal ports from which terminals are modeled
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
- multiPort (
ProcessBuiltInPaths¶
-
SegmentManager.
ProcessBuiltInPaths
¶ Create segments of
NXOpen.Routing.BuiltInPath
objects present in thisNXOpen.Assemblies.Component
object.Signature
ProcessBuiltInPaths(partOcc)
Parameters: partOcc ( NXOpen.Assemblies.Component
) –New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
SetFollowCurve¶
-
SegmentManager.
SetFollowCurve
¶ Set segment follow curve.
Segment can change type to mirror the type of the follow curve being set.
Signature
SetFollowCurve(segment, followCurve)
Parameters: - segment (
NXOpen.Routing.ISegment
) – Segment to set follow curve on - followCurve (
NXOpen.Curve
) – Follow curve of segment
Returns: Segment can possibly change types.
Use the returned segment object pointer instead of any older pointers after calling this function. For example: A LineSegment can become a SplineSegment after calling this function if new follow curve is a spline. :rtype:
NXOpen.Routing.ISegment
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
- segment (
SimplifySegments¶
-
SegmentManager.
SimplifySegments
¶ Combine segments that are collinear and whose intermediate RCPs do not branch
Signature
SimplifySegments(segments, doUpdate)
Parameters: - segments (list of
NXOpen.Routing.ISegment
) – segments to combine - doUpdate (bool) – Fires update if True
Returns: resulting segments
Return type: list of
NXOpen.Routing.ISegment
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
- segments (list of
Subdivide¶
-
SegmentManager.
Subdivide
¶ Subdivide a routing path segment
Signature
Subdivide(segment, subdivideOption)
Parameters: - segment (
NXOpen.Routing.ISegment
) – Segment to subdivide - subdivideOption (
NXOpen.Routing.SegmentManagerSubdivideOption_Struct
) –
Returns: resulting segments
Return type: list of
NXOpen.Routing.ISegment
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
- segment (
UnmodelTerminals¶
-
SegmentManager.
UnmodelTerminals
¶ Un-model terminals and update connection list routes for specified terminal ports.
Signature
UnmodelTerminals(multiPort, terminalPorts)
Parameters: - multiPort (
NXOpen.Routing.Port
) – MultiPort whose terminals being un-modeled - terminalPorts (list of
NXOpen.Routing.Port
) – Terminal ports being modeled
New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
- multiPort (