BranchPathNumberingBuilderSequence Enumeration¶
NXOpen.Routing.BranchPathNumberingBuilder.Sequence is an alias for NXOpen.Routing.BranchPathNumberingBuilderSequence
-
class
NXOpen.Routing.
BranchPathNumberingBuilderSequence
¶ Bases:
object
Specifies the sequence method
Enum Members
Enum Member Enum Member Description Numbers 1, 2, 3,.....UpperCase A, B, C,.....LowerCase a, b, c,.....-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-