FillerCollection Class¶
-
class
NXOpen.Routing.
FillerCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.Stock
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateStock | Creates a NXOpen.Routing.Filler stock object. |
Method Detail¶
CreateStock¶
-
FillerCollection.
CreateStock
¶ Creates a
NXOpen.Routing.Filler
stock object.Signature
CreateStock(stockData, anchor, crossSection, segments)
Parameters: - stockData (
NXOpen.Routing.StockData
) – TheNXOpen.Routing.StockData
that defines the stock - anchor (
NXOpen.Routing.Anchor
) – TheNXOpen.Routing.Anchor
from the inputNXOpen.Routing.StockData
to use, ja_NULL is allowed for no anchor. - crossSection (
NXOpen.Routing.CrossSection
) – TheNXOpen.Routing.CrossSection
from the inputNXOpen.Routing.StockData
to use, ja_NULL is not allowed. - segments (list of
NXOpen.Routing.ISegment
) – The array ofNXOpen.Routing.ISegment
curves that the stock must cover.
Returns: The resulting array of newly created
NXOpen.Routing.Stock
objects. :rtype: list of
NXOpen.Routing.Stock
New in version NX4.0.0.
License requirements: routing_harness (“Routing Harness”)
- stockData (