EditLineSegmentBuilder Class¶
-
class
NXOpen.Routing.
EditLineSegmentBuilder
¶ Bases:
NXOpen.Builder
Builder for the “Edit Line Segment” operation.
Sets (and locks or unlocks) the length of
NXOpen.Routing.LineSegment
objects. Also moves geometry attached to the line segment to ensure that the attached geometry has the correct shape after an edit.To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateEditLineSegmentBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ConvertEccentricSegment | Returns or sets the conversion flag. |
Length | Returns the length expression. |
LineSelection | Returns the line selection. |
LockLength | Returns or sets the lock length flag. |
ReverseDirection | Returns or sets the reverse direction flag. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddLineToSetOfAllEditedSegments | Adds the current line segment to the set of all line segments that have been edited by the user. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DetachActiveRcp | Detaches the line segment, stored in builder, at its active end RCP. |
DragLineLength | Updates the line length based on the expression stored in this builder. |
GetActiveRcpPositon | Determines the active RCP for the line selected by the user. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOrientation | Determines the orientation information for the line selected by the user. |
InitializeFromLine | Initializes (or resets) the builder based off of the input line segment. |
ModifiedLineLength | Updates the line length based on the expression stored in this builder. |
RestartDrag | Restart a line drag operation. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
StopDrag | Stop the drag operation if it has begun. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ConvertEccentricSegment¶
-
EditLineSegmentBuilder.
ConvertEccentricSegment
¶ Returns or sets the conversion flag.
Forces the commit method to convert line segment to eccentric line segment if set to true. Otherwise convert it to vice versa
-------------------------------------
Getter Method
Signature
ConvertEccentricSegment()
Returns: Return type: bool New in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ConvertEccentricSegment(convertEccentricSegment)
Parameters: convertEccentricSegment (bool) – New in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
Length¶
-
EditLineSegmentBuilder.
Length
¶ Returns the length expression.
This data from this expression is copied to (or from) the distance constraint applied to the ends of the line segment.
-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
LineSelection¶
-
EditLineSegmentBuilder.
LineSelection
¶ Returns the line selection.
Stores the line segment selected by the user.
-------------------------------------
Getter Method
Signature
LineSelection()
Returns: Return type: NXOpen.Routing.SelectLineSegment
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
LockLength¶
-
EditLineSegmentBuilder.
LockLength
¶ Returns or sets the lock length flag.
Forces the commit method to lock the length to the specified value if set to true. Otherwise the length of the line segment is unconstrained after the commit method is invoked.
-------------------------------------
Getter Method
Signature
LockLength()
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
LockLength(lockLength)
Parameters: lockLength (bool) – New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
ReverseDirection¶
-
EditLineSegmentBuilder.
ReverseDirection
¶ Returns or sets the reverse direction flag.
Flips the direction that the extends towards (or shrinks along). This flips the origin of the line as well as the direction.
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ReverseDirection(reverse)
Parameters: reverse (bool) – New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
AddLineToSetOfAllEditedSegments¶
-
EditLineSegmentBuilder.
AddLineToSetOfAllEditedSegments
¶ Adds the current line segment to the set of all line segments that have been edited by the user.
Signature
AddLineToSetOfAllEditedSegments()
New in version NX9.0.2.
License requirements: routing_base (“Routing Basic”)
DetachActiveRcp¶
-
EditLineSegmentBuilder.
DetachActiveRcp
¶ Detaches the line segment, stored in builder, at its active end RCP.
By reversing the direction of line segment, user could make other end RCP as active RCP.
Signature
DetachActiveRcp()
New in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
DragLineLength¶
-
EditLineSegmentBuilder.
DragLineLength
¶ Updates the line length based on the expression stored in this builder.
The line is not fully updated only partially updated (i.e. solid bodies build on the line do not update). This method assumes the difference between the new length value and the previous length value is very small (e.g. a drag operation).
Signature
DragLineLength()
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
GetActiveRcpPositon¶
-
EditLineSegmentBuilder.
GetActiveRcpPositon
¶ Determines the active RCP for the line selected by the user.
This is end RCP other than the start point of line segment. This RCP could be dragged along the segment.
Signature
GetActiveRcpPositon()
Returns: End point other than the start point of line segment. :rtype:
NXOpen.Point3d
New in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
GetOrientation¶
-
EditLineSegmentBuilder.
GetOrientation
¶ Determines the orientation information for the line selected by the user.
Returns false if there is no line currently stored in the builder.
Signature
GetOrientation()
Returns: a tuple Return type: A tuple consisting of (isValid, startPoint, direction). isValid is a bool. True if there is a line associated with this builder. startPoint is a NXOpen.Point3d
. The start of the line. direction is aNXOpen.Vector3d
. The direction of the line (unit vector).New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
InitializeFromLine¶
-
EditLineSegmentBuilder.
InitializeFromLine
¶ Initializes (or resets) the builder based off of the input line segment.
Signature
InitializeFromLine(line)
Parameters: line ( NXOpen.Routing.LineSegment
) – Line object, may be NoneNew in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
ModifiedLineLength¶
-
EditLineSegmentBuilder.
ModifiedLineLength
¶ Updates the line length based on the expression stored in this builder.
The line is not fully updated only partially updated (i.e. solid bodies build on the line do not update). This method doesn’t assume anything about the new value. This method updates the line incrementally from the original length to the new length as this usually results in better looking geometry.
Signature
ModifiedLineLength()
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
RestartDrag¶
-
EditLineSegmentBuilder.
RestartDrag
¶ Restart a line drag operation.
This routine should only be called if
NXOpen.Routing.EditLineSegmentBuilder.StopDrag
. was previously called to stop a line drag operation.Signature
RestartDrag()
New in version NX7.5.1.
License requirements: routing_base (“Routing Basic”)
StopDrag¶
-
EditLineSegmentBuilder.
StopDrag
¶ Stop the drag operation if it has begun.
This will commit the drag and update the assembly. This will not remove the segment from the builder and dragging can be restarted by calling
NXOpen.Routing.EditLineSegmentBuilder.RestartDrag
.Signature
StopDrag()
New in version NX7.5.1.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
EditLineSegmentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.