RouteSweptTwistBuilder Class¶
-
class
NXOpen.Routing.
RouteSweptTwistBuilder
¶ Bases:
NXOpen.Builder
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateRouteSweptTwistBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Spine | Returns the spine |
Stock | Returns the stock |
Tag | Returns the Tag for this object. |
TwistPoint | Returns or sets the twist point |
TwistPointList | Returns the twist point list |
Methods¶
Method | Description |
---|---|
AskExistingTwistData | The twist data i. |
Commit | Commits any edits that have been applied to the builder. |
CreateSpine | Creates a new spine |
CreateSpinePoint | Creates a new spine point @return OnPathDimWithValueBuilder Object |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Spine¶
-
RouteSweptTwistBuilder.
Spine
¶ Returns the spine
-------------------------------------
Getter Method
Signature
Spine()
Returns: Return type: NXOpen.Curve
New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
Stock¶
-
RouteSweptTwistBuilder.
Stock
¶ Returns the stock
-------------------------------------
Getter Method
Signature
Stock()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
TwistPoint¶
-
RouteSweptTwistBuilder.
TwistPoint
¶ Returns or sets the twist point
-------------------------------------
Getter Method
Signature
TwistPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
TwistPoint(twistPoint)
Parameters: twistPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
TwistPointList¶
-
RouteSweptTwistBuilder.
TwistPointList
¶ Returns the twist point list
-------------------------------------
Getter Method
Signature
TwistPointList()
Returns: Return type: NXOpen.TaggedObjectList
New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
Method Detail¶
AskExistingTwistData¶
-
RouteSweptTwistBuilder.
AskExistingTwistData
¶ The twist data i.
e locations and angles
Signature
AskExistingTwistData()
Returns: a tuple Return type: A tuple consisting of (locations, angles). locations is a list of float. Number of locations angles is a list of float. Number of angles New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
CreateSpine¶
-
RouteSweptTwistBuilder.
CreateSpine
¶ Creates a new spine
Signature
CreateSpine()
New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
CreateSpinePoint¶
-
RouteSweptTwistBuilder.
CreateSpinePoint
¶ Creates a new spine point
Signature
CreateSpinePoint()
Returns: OnPathDimWithValueBuilder Object Return type: NXOpen.GeometricUtilities.OnPathDimWithValueBuilder
New in version NX6.0.0.
License requirements: routing_harness (“Routing Harness”)
Validate¶
-
RouteSweptTwistBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.